Member's Forum What would you put in a solder aid or emergency maker kit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 626 subscribers
  • Views 30890 views
  • Users 0 members are here
Related

What would you put in a solder aid or emergency maker kit?

scottiebabe
scottiebabe over 3 years ago

If you are away from your workbench either in your backyard or perhaps 100's km away and you need to repair or modify your project or prototype what would be the essential tools and components needed?

I am taking some inspiration from these low cost 100-in-1 solder tool kits:

image

Here is my Second Draft Attempt:

Tools Consumables Components Electronics Jellybeans Tin
Portable soldering iron Solder (Your choice leaded) USB Wall Wart spdt switch
Solder sucker Solder braid USB Power Bank banana jack
Multimeter Heat shrink USB A - micro cable banana plug
Ruler Hot glue stick USB C - C cable 1n4007 x4
Wire strippers (your-choice) Zip-ties 100 thou headers 1N4148
Side cutters Tape (your-choice) Dupont jumpers 2n3904/2n3906
Pliers Flux A piece of perf board Power N-FET
Tweezers Bismuth Solder A piece of copper clad board Axial Resistors 100,1k,10K,100K Qty 10 each
Telescoping Magnet  Flux A piece of 1.5 mm plywood Some leaded LEDs
Knife (not sure what kind)  Cyanoacrylate Glue Hookup wire (24AWG stranded likely) 7805
Bic lighter Heat Sink Sil-Pad 10 cm of cat-x network cable LM317 and potentiometer
Miniature screw driver set (the interchange bits)   small spool of 30AWG Kynar wire A few electrolytic capacitors
Alligator clip leads Copper Tape Tin of Electronics Jellybeans LM324 or LM358
Soldering Iron Stand Polydoh RPI Pico 0805 SMD Assortment
Tip Cleaner (your-choice) Blu-tac extension cord
Sharpie Stress-relieving candy power bar
Flash Light Electronics Cleaner 9V battery
Safety Glasses ESD Bag 4-40 machine screws
  Nail Polish
 
Plastic Prying 
Spudger
Scissors
Vise Grips
crescent wrench
Full Size Screw drivers
Helping Hands
Earth Ground Plug
ESD Mat
ESD Wrist Strap

I have pretty much all of these items in quantity already. So I can easily appropriate some of them to my emergency maker kit! Like wind the wires listed onto a small bobins, etc

baldengineer is also ahead of me with 0805 smd components suggestion! 

I'm trying to not go overboard with handtools but I think I could use some more...

Perhaps there are low cost modules you shouldn't leave home without? lol...

This is definitely a work in progress...

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 3 years ago in reply to dougw

    I've got test leads that have similar clips, they implemented the wiring slightly differently, coming out one end of each clip (i.e. looping one wire in a U-shape to reach the other side from inside).

    Photo on my fancy mouse pad : 

    image

    I don't think they did anything apart from soldering them and then a bit of heatshrink, but I've not cut them apart to see what they did, because I use these clips. I think they just expect it to last a while, long enough for the wear-and-tear to not be significant perhaps.

    Here's a photo of the inside of an unused one (same type) (to anyone who is not familiar with these, the copper part is the terminal with some solder already on it, and the other metal piece is just part of the spring that holds the clips closed).

    I don't know if it would work, but maybe pack the cable with a bit of sleeving, and then as Dave says use a cable tie (could make a couple of notches on the inside for that). The head of a small cable tie could then be on the inside, and it wouldn't interfere with the other side, because the two cables would egress from the one side. This cunning plan may or may not work : ) 

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to dougw
    dougw said:
    How would you tackle this build?
    • sleeved grommets in the end of the clip handles
    • test lead sockets in the end of the clip handles
    • cable tie through the plastic, around the cable, and back through the plastic

    Perhaps a little less glue Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    image i'm covered

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 3 years ago in reply to shabaz

    I would hot glue more if I were better at it.  It could be that I need a better tool as I always have problems with dripping, but it's probably just me.  I guess I'm impatient too because it takes a while for the glue to set up (it could be that I get it too hot).

    Maybe I'll get a USB gun and see if I can do better.  If I could apply the hot glue with some precision, I think that I'd use it with some of my 3D prints, but I doubt if I would ever get that to work.

    My wife uses it successfully for crafting, so it's probably just a skill issue.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to scottiebabe

    I recently used hot glue to fashion a strain relief (along with heatshrink) when connecting wire to a Kelvin clip - the wire needed to be immobilized to prevent stress on the solder joint:

    image

    Sometimes it is hard to beat the hot glue solution.

    How would you tackle this build?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Same here, I have a hot glue gun and it's been used zero times so far, I'm just not experienced enough with that glue to know the situations to use the tool, since there are usually other adhesives around.

    Regarding hot air tool, I do a similar thing with Polydoh (it's supposed to be softened in boiling water, but hot air tool works better for small quantities of the pellets.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to ralphjy

    Its pink! and cordless! Great find!

    image

    I knew there were cordless ones based on large tool batteries but not these miniature ones

    image

    Great find thanks for sharing Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    I don't hot glue enough for a glue gun to make it into the emergency kit, but I can see others justifying having it in their kit. Most of the time I heat up the end of a glue stick with hot air or a lighter than put a big gob to hold something down. When I hot glued a thermistor to a solar panel I used a magnifying glass to heat up the hot glue, no batteries required! 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 3 years ago in reply to dougw

    Have you tried a USB one?  Seems to be quite a few different models and I wonder which ones work well.  Reviews on Amazon seem okay.

    Pink USB Hot Glue Gun that someone might like Grinning.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>