Member's Forum How do you make reliable, low-cost cables quickly?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 52 replies
  • Subscribers 624 subscribers
  • Views 6075 views
  • Users 0 members are here
  • dougw
  • bootlace connectors
  • custom cables
  • MTA
  • Yodamonk
Related

How do you make reliable, low-cost cables quickly?

dougw
dougw over 2 years ago

I do lots of electronics design and building and inevitably need to make lots of cables. Since making cables is not my favorite activity, I try to use methods that are quick while still providing reliable connections. And of course I always need to keep the costs down.

This short post shows a couple of the main ways I accomplish these objectives.

image

Yodamonk, the cable guru.

Custom Cable Methods

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

I haven't posted much content lately so I thought I would post something about making cables. This activity is not usually exciting enough to be a great blogging topic, but I also wanted to play around a bit with some AI media generation. (No AI text though) The tough Yodamonk dude came out amazing.

I am always looking for efficient ways to make useful cables, so if you have any interesting tips, please jot them down below...

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave

    It's a pity most of the desk microphones in such systems are now carried over unshielded twisted pair.. I used to use the old ones as a good source of high-quality shielded audio cable! My old ebay search terms are getting rare, so if you know of any more models as search terms, that would be great to know : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz
    shabaz said:
    but that's a good point, there are less common variants to  eliminate risk of accidentally plugging the wrong thing in

    The RJ45 and RJ50 can be still be plugged into each other. The RJ50 just has the additional outer pins.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz
    shabaz said:
    that photo is not an Axis camera connector

    Nope, it is the end of a Sennheiser ADN Digital Conference System cable. They use RJ50 instead of RJ45 (but wired as RJ45) to daisy chain the microphone units back to the control system.

    shabaz said:
    Impressive close-up!

    Yes, I thought that as well. I got it for 24/7 live network streams of experiments and the like. Unlike the M10 series, the M11 series have interchangeable lenses, so you have more flexibility. That was just with the supplied lens however.

      

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz
    shabaz said:
    Also sometimes RJ45 is used for (ancient) telecoms protocols,

    There was the RJ45S variant which has the additional key on the side.

    https://en.wikipedia.org/wiki/Registered_jack#RJ45S

    Stops you from plugging RJ45S cables into RJ45 equipment but not the other way around.

    shabaz said:
    But hard to get away from RJ45

    The issue I have is to prevent people plugging RJ45 connectors into the wrong outlets in floor boxes and wall plates.

    Even if I use Ethercon, sooner you will find a non-Ethercon cable plugged into it instead of the normal outlet next to it and the support desk phone call to say it's not working.

    I have looked at M12, but a bit on the large side for some set-ups.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave

    Just understood your comment.. that photo is not an Axis camera connector, but the photo was taken _with_ an Axis camera?! Impressive close-up!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave

    I have hundreds of RJ45 connectors to use up first, but that's a good point, there are less common variants to  eliminate risk of accidentally plugging the wrong thing in.

    There's a small amount of precedent for non-Ethernet with RJ45, I think I saw some device with a very recessed RJ45, that needed a specially moulded cable shape to fit it. Also sometimes RJ45 is used for (ancient) telecoms protocols, e.g. some ISDN variants can use it I think, even with the same moulded latch position.

    For copper connections (i.e. excluding fiber), I've seen Ethernet carried over circular connectors (e.g. M12 is popular for that), for certain industries (railway etc). But hard to get away from RJ45, even industrial products use it. It's a connector that simply got to be more and more useful over time, as even more things were sent over it. Some people use it (almost) purely for power, with the Ethernet function of it still used, but barely.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz
    shabaz said:
    A bit naughty, but I like using RJ45 for non-Ethernet stuff too, as long as it is labeled clearly.

    You could perhaps use RJ50 to keep your conscious clear Slight smile

    image

    (FYI the photo was taken with an Axis M1135 CCTV camera) 

    Have you used any other connectors for Ethernet ? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 2 years ago in reply to BigG

    I also haven't tried this, but Ian Lesner from Dangerous Prototypes (The Bus Pirate creator) has a portfolio of electronics related services. It mainly started with Dirty PCBs, but also Dirty Cables. He has been at least twice on the Amp Hour podcast, but I can't find the latest episode (i believe it was 2024 after releasing Bus Pirate 5).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    I wish there was a source of good quality but low-cost pre-assembled audio cables. All the consumer stuff is low-quality, and all the studio grade cables are pricey.

    I end up DIY'ing them and it takes quite a while.

    Mini-XLR cable I had to assemble today.

    image

    image

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to ntewinkel

    They are excellent connectors + cable. Also one of the cheapest ways of obtaining prototyping wire at low cost, just strip off the outer jacket.

    Here I think the ready-made stranded wire patch cables cost a bit more than DIYing them (assuming the typical ratchet tool is available), but either way, they are low-cost. Solid-core wire plus the plastic tool is often used for the fixed wiring install. A bit naughty, but I like using RJ45 for non-Ethernet stuff too, as long as it is labeled clearly. Major benefit being that the patch cables are ready-made so no time wasted assembling cables.

    I also like circular connectors (since it's so easy to drill round holes for those!) but I don't have a favorite. Pity some of those connectors can be pricey, whereas RJ45 is super-low-cost.

    The tool I've used for > 10 years. It does 4 and 6-way connectors too, but I rarely use those.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>