Member's Forum 8-gang individually switched power strips hard to come by?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 632 subscribers
  • Views 1660 views
  • Users 0 members are here
Related

8-gang individually switched power strips hard to come by?

Andrew J
Andrew J over 7 years ago

Well so it would seem.  If I wanted a rectangular 4x4, individually switched, surge protected extension lead, no problem.  If I wanted a 8x1 surge protected extension lead, no problem.  But a 8x1, 3-metre, individually switched, surge protected extension lead seems to be non-existent.  Has anyone come across anything like this - perhaps has better Google-fu than me?  UK socket.

 

On eBay, 166BatteryWorld are selling a configurable tower with 4 gang-per-layer (or 2-gang + 2-usb socket layer) which might work: although only a layer (4 sockets) are switchable.  https://www.ebay.co.uk/itm/3M-Switched-Surge-Protected-Extension-Lead-UK-Plug-Tower-Multi-Socket-4-USB-Port-/32366697679…

I've not heard anything about them, they purport to ship from Portsmouth in 1 day yet are a Chinese company: we've all heard the horror stories about chinese-sourced power supplies when non-branded so I'd be a little concerned.  There are lots of sellers with the equivalent which doesn't help with confidence either.  Has anyone had any dealings with them?

 

Thanks,

 

Andrew

  • Sign in to reply
  • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to 14rhb

    To be honest Rod, I don't want to mess around with mains voltage/current at the moment. 

     

    I want 2 for different purposes.  One of them will be used to plug in my iMac, MacBook, printer, phone, disk drive, Sonos bridge, router with one to spare - perhaps a second monitor.  That can sit at one end of my work area, out of the way and, to be fair, that doesn't need to be individually switchable as I never turn any of that stuff off currently anyway.  The second will be for a fibre modem (because of location!), daylight lighting and other stuff I start playing with such as power supply, oscilloscope etc.  At the moment, I'm continuously plugging/unplugging a 9v/12v power supply that I use for experiments, because it doesn't have a power switch, and an earthing plug and it would be easier if the former could just be switched on/off as needed.  It also made me think that if the other sockets were switchable, I could ensure that I didn't exceed power limits on the supply by accident, even given that most of those types of devices have a power switch, if that makes sense.

     

    Perhaps I'm being ambitious in that?  Possible - I wouldn't want to do anything dangerous, so general advice might be for that type of equipment get something like the Olsen ones Dave has linked to.  Although those look ideal and are undoubtedly high quality, £240+ for power strips is a bit more than I wanted to spend.  I could probably get one of those and a more bog-standard non-switchable one for the 'potaahs, drives and stuff, although even one is pushing what I want to spend.  The eBay one's look like they might do but, as I say, I've heard a fair few horror stories about non-branded Chinese power supplies so I'm a bit wary.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to Andrew J

    Here is a bespoke one they made for me some time ago. There's just never enough outlets these days...

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    Hi Andrew,

     

    Does it have to be a ready made product i.e. because you need many of them to incorporate into a design or it needs to be certifiable for use in public places/education establishments etc. If not then you could buy four double socket outlets Iindividually switched) and mount them in a line using dual gang surface mount boxes - you'd need to add internal wiring/ gromets between the boxes and find something suitable to mount them to (personally a nice peice of plywood would be my choice but again would likely fall foul of any electrical inspection for non-combustible backing board ).

     

    I think the Ebay companies you mention are often owned by international operators but they have already imported stock to key locations in other countries (in your case the UK), from experience they do normally deliver quite quickly (make sure you confirm from the delivery dates in Ebay).

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to beacon_dave

    That's the ticket.  Let me just have a word with the Bank Manager image!  I might have to hold out for something cheaper if I'm honest, but that's pretty much a spec of what I'm after.  Thanks Dave.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago

    Perhaps speak to Olson...

     

    https://olsondirect.co.uk/8-way-13a-individually-switched-neon-fused-pdu.html?___SID=U

     

    they can do bespoke.

     

    Alternatively swap the plug for a surge protected plug-cap

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<