This is a teaser of the pinball machine I am working on.
And yes this is my first and I do know that the flippers need to be adjusted so that they do not hit the slings at the bottom. Lol
On Update 12 I have the PCB side and the schematic side by side.
And this is the flipper control board not the main power supply or the transformer.
It is to get the flippers to work which take 50 Volts to run them.
And I know about Contry voltages I have 4 pinball machines I've worked on for the expeeriance.
2 EM's and 2 80s SS pins.
Curious of why you decided to use 50VAC input side when most places use 120VAC in US or 240VAC EU/ASIA? Great looking board. Does it come with a schematic?
Thanks,
Clem
I will need help on the boards.
I am wanting it like an 80s and 90s pinball machine where the boards are separate but with better efficient components etc.
I have up on the latest Kickstarter Update a concept art of the flipper power supply.
The kickstarter link is: https://www.kickstarter.com/projects/pinballreviewer/fursona-land-custom-pinball-machine
The name is inspired by Police Force with the all Anthro charactors on the cab and playfield.
I have lots of reward tiers and lots of updates.
I have a Kickstarter up for it now.
It is https://www.kickstarter.com/projects/pinballreviewer/fursona-land-custom-pinball-machine
And the name for it is inspiration of Police Force made by Williams.
And there are 12 reward tiers $50 gets a pretty cool Kickstarter only glass and $500 gets a Kickstarter only Topper.
If you cannot help just spread the word.
Great project. Ask when you need help here.
C
Top Comments