Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Checking Out GaN Half-Bridge Power Stage: Texas Instruments LMG5200 - Part 2: Dead Time Capture
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 3 Sep 2015 6:04 PM Date Created
  • Views 4783 views
  • Likes 7 likes
  • Comments 8 comments
  • lmg5200
  • dead_time
  • half_bridge
  • texas_instruments
  • gan
  • half_bridge_drivers
  • fet
Related
Recommended

Checking Out GaN Half-Bridge Power Stage: Texas Instruments LMG5200 - Part 2: Dead Time Capture

Jan Cumps
Jan Cumps
3 Sep 2015

It doesn't have to be silicon all the time. I have a Gallium-nitride device here at the Cumps lab that I'm going to try out. In some high voltage, high power designs, GaN FETs have advantages over Si. On the other hand they are also more difficult to drive.

 

The chip that I have contains a built-in smart GaN FET driver. That takes away the complexities of driving the power stage correctly. We're covering fairly new technology here. The documents are still marked technology preview. I received them from TI after attending a GaN seminar and answering right on the quiz.

 

In this post I'm probing the switching output and checking the dead time between switching transitions.

 


image

 

The Switching Node Output

 

image

 

Taken from the technology preview document lmg5200.pdf.

 

The switching node (pin 8, SW in the schema above) is the output tab between the upper and lower half of the half-bridge.
It's the power output signal - driven high and low by the two output FETs to generate the final PWM.
Between the transitions there has to be some dead time - a time when it's guaranteed that both sides of the bridge are shut off.

To allow fast switching times, it's key to optimize the dead time. It should be long enought to ensure stability, but no longer.

In an optimal configuration, one side of the bridge is always on and one side off.
Dead time eats away from that optimal situation and limits the maximum PWM frequency.

 

What is Dead Time?

Definition from Infineon AN2007-104 Dead Time Calculation for IGBT modules (this applies to GaN modules too):

 

In order to avoid bridge shoot through it is always recommended to add a so called “interlock delay time” or more popular “dead time” into the control scheme. With this additional time one IGBT will be always turned off first and the other will be turned on after dead time is expired, hence bridge shoot through caused by the unsymmetrical turn on and turn off time of the IGBT devices can be avoided.

 

The GaN driver that I'm using here, where the driver logic is built into the same package as the GaN power FETs, allows for dead times smaller than 10 ns.

On my evaluation board, the dead time is configured to be approx 8 ns. Let's probe that!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Test Setup

 

The evaluation guide of my board gives a detailed overview of how to do these measurements.

We're talking about fast edges here, so our test setup has to be done right to avoid introducing parasitic inductance via our probe.

Ever wondered why there's a spring in the accessories bag of your scope? It's there to do measurements like this, at frequencies where the ground wire of the scope can act as an extra inductor or as a noise antenna.

The ground spring minimizes that loop.

 

I've measured two signals: the dead time when switching the output from low to high, and - just for kicks - the rise time of the output PWM.

I'm measuring a dead time of 7.2 ns. Almost the 8 ns specified in the doco.

image

 

The rise time - measured just before the output LC filter, with 1 amp output load, 50% duty cycle, is 3.8 ns.

image

We're dealing with a fast switcher here. That opens new opportunities for small high-power switching.

But it's also going to cause some headaches on the EMF compliance front.

 

Related Posts
Part 1: Preview
Part 2: Dead Time Capture
Part 3: Control Deadband with Hercules LaunchPad

Hercules LaunchPad and GaN FETs: Control Big Power with a Flimsy Mouse Scroll Wheel

on TI E2E community: driving GaN with a simple PWM signal
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago +2
    TI published an article I wrote about driving GaN on their E2E community blog: https://e2e.ti.com/blogs_/b/powerhouse/archive/2015/09/10/control-a-gan-half-bridge-driver-with-a-single-pwm-signal https…
  • DAB
    DAB over 11 years ago +1
    I am curious, did you have a fast enough scope to see any high frequency ringing for that fast of a current rise? I am not sure if the real waveform would be that smooth or if there is some filtering going…
  • jw0752
    jw0752 over 11 years ago +1
    Thank you Jan, I learned several new things by reading and watching your video. This type of experiment is really great. John
  • jw0752
    jw0752 over 11 years ago

    Thank you Jan,

    I learned several new things by reading and watching your video. This type of experiment is really great.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to DAB

    My scope isn't fast enough. In the evaluation manual that's refered to in my post, you can find a capture with a faster scope. There's significant ringing visible there.

    The scope is good enough to measure the dead time. But that's it - limits reached.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    I am curious, did you have a fast enough scope to see any high frequency ringing for that fast of a current rise?

     

    I am not sure if the real waveform would be that smooth or if there is some filtering going on.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<