Personal Blogs
  • Members
  • More
Personal Blogs
Legacy Personal Blogs LED Floodlight 80W
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Former Member
  • Date Created: 28 May 2012 8:04 AM Date Created
  • Views 514 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

LED Floodlight 80W

Former Member
Former Member
28 May 2012

LED fluorescent lamp with its unique advantages more and more into people's lives. This light is what What are the advantages? Today we inventory.

First, led driver 120w       fluorescent lamp does not use mercury, and which do not lead, and contains large amounts of mercury vapor in the traditional fluorescent lamp, this lamp broken mercury vapor is evaporation into the atmosphere, thereby polluting the environment, LED fluorescent can be good to protect the environment, is recognized as a green light.

Secondly, LED Floodlight 80W    fluorescent lamp is a cold light source, not like traditional lamps that emit large amounts of heat. Basically, it can electrical energy converted to light, will cause the waste of energy, very economical.

Again, LED fluorescent lamp is a very quiet and energy-saving lamps, not the same as traditional fluorescent noise, very suitable for the need for a quiet environment, such as libraries, offices and the like place. Also a good eye protection, start very fast, no flickering, very beneficial to our health.

In addition, LED Flood light 10W  fluorescent green lamps, which itself does not produce ultraviolet light, infrared radiation, do not contain mercury and other harmful substances, less heat, and avoid the mosquitoes around in next to the light source, This gives the room to create a clean environment.

Finally, the service life of the LED Power Supply  fluorescent lamp is very long, its power consumption is less than one-third of the traditional fluorescent lamp, but the brightness is consistent with the traditional fluorescent. In general, the normal life of 30 000 hours or more, long-term use without replacement, invisibly to reduce labor costs, it is suitable for the occasion of some inconvenience to the replacement of lamps. Of course, the color of the LED Spotlight 30W  fluorescent lamp is very rich, you can create a variety of light-emitting colored lights, to meet the needs of different occasions.
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
An Avnet Company © 2023 Premier Farnell Limited. All Rights Reserved.