Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Makevember++ : A Christmas LED Decoration
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 2 Dec 2019 5:40 PM Date Created
  • Views 1633 views
  • Likes 11 likes
  • Comments 13 comments
  • nano
  • led christmas tree
Related
Recommended

Makevember++ : A Christmas LED Decoration

dubbie
dubbie
2 Dec 2019

I know that it is now December but I still have one more Makevember project to include, which I mostly did in November, so I have made it a Makevember++ Project. It is just 7 white LEDs arranged in the abstract shape of a Christmas tree. I 3D printed a former to hold all the LEDs in place which was designed as an interference fit into a small wood frame canvas used for art. Unfortunately the wood frame I used for measurements is an older one I have already used and the newer ones, although the same outer size, have a larger inner size as they use less wood (persumably to save money). So instead of a good movement free interference fit there is no fit at all. So I just BlueTac'ed it in place. I might make a new 3D printed former as now there is probably room for a couple more LEDs. I considered using different coloured LEDs, to be more like the baubles on a Christmas tree, but they all had different brightnesses, different current levels and different on voltages. The whites looked nice so I just went with white.

 

I connected the LEDs up directly to the outputs of an Arduino Nano that Element14 sent me for an earlier Makevember project. The LEDs all have a common ground and are driven by a HIGH on a digital output pin. I did this as it means if the power voltage drops then all the LED voltages will drop equally so that the relative brightness levels will be maintained. It also means that If battery powered that as the voltages drop the LEDs will use less current and the life of the battery will be extended, albeit the LEDs will be dimmer. They are pretty bright now with a 1 kOhm series resistor so this should work for a while. I have not yet worked out the predicted life of the LED tree when using a specific battery set.

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Dubbie

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 6 years ago +4
    That mini easel frame could work quite well with a small E-Ink type display. Have it update its contents overnight like an advent calendar to reveal a new image or message the following morning. The picopower…
  • genebren
    genebren over 6 years ago +4
    Clever little Christmas tree display! A few more LEDs (all RGB leds) and you would have a bit more flexible display.
  • dubbie
    dubbie over 6 years ago in reply to beacon_dave +2
    What a great idea - I hadn't thought of anything like that. I wonder if I can get an e-ink display before Christmas! One of my next steps is to get a programmer for ATTing85 microcontrollers implemented…
  • dubbie
    dubbie over 6 years ago in reply to beacon_dave

    What a great idea - I hadn't thought of anything like that. I wonder if I can get an e-ink display before Christmas! One of my next steps is to get a programmer for ATTing85 microcontrollers implemented, specifically so that I can make low powered versions of my LED displays. Hopefully, I will manage this, this Christmas (I've been planning to do this for the last three Christmas's).

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 6 years ago

    Clever little Christmas tree display!  A few more LEDs (all RGB leds) and you would have a bit more flexible display.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago

    That mini easel frame could work quite well with a small E-Ink type display. Have it update its contents overnight like an advent calendar to reveal a new image or message the following morning. The picopower modes of an Atmel microcontroller could keep it running all through the festive season from a small power pack.   

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<