Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Problems soldering micro usb connectors
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: camuyano
  • Date Created: 2 Mar 2016 12:21 PM Date Created
  • Views 4687 views
  • Likes 3 likes
  • Comments 13 comments
  • smd
  • pcb
  • usb
  • soldering
Related
Recommended

Problems soldering micro usb connectors

camuyano
camuyano
2 Mar 2016

Currently I am working building a board that uses a micro USB female connector. In theory this was amazing until I had to hand solder those diabolic connectors. The pins are tiny and very short and that makes my success rate of soldering the connectors down to something like 4 good out of 5 tries. After looking some soul searching for the roads of the internet I found on Adafruit's site someone pointing to the trinket board connector. So I decided to go with it, I went into the trinket github and just copy pasted the part to my design and sent the PCB to fab. In a few weeks I should receive the board and some connectors and give it a try.

Here is a picture of the connector I will be trying out. It  seems to be easier than the other however this has to go trough the PCB so I cannot have much on the other side of the PCB. Current PCB had some extra real state but maybe not so in others.

 

image

 

 

If anyone has tips and tricks on how to solder microusb connectors by hand let me know. For now I am just practicing and practicing and practicing. Logic says that if I practice enough eventually I will be able to clean solder them.

Also how about strong holds of the connectors, what is a recommended connector that can withstand some abuse.

If all goes well I will be soldering about 200 of them, maybe after I will have all the practice I need.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago +1
    Hi! Hot air gun, solder paste and good cleaning before soldering. Tom
  • shabaz
    shabaz over 10 years ago +1
    By hand it takes me too long to solder a single microUSB to want to do many of them. That is with a soldering iron; presumably much, much easier with reflow but I've not tried that with such connectors…
  • mlease
    mlease over 10 years ago in reply to camuyano +1
    Javier, get a small tube of solder past. Smear a little of the solder paste on the pins of the connector and then place it on the board. You do need a fairly fine pointed soldering iron tip but just place…
  • mlease
    mlease over 10 years ago in reply to DAB

    To expand on DAB's comments, it really depends on the board plating and if you are using solder "wire" or paste. I've done a lot of soldering on HASL finished boards with solder paste and rarely have problems with solder flow or joint quality. Boards with something besides HASL finish are definitely trickier and will benefit from pre-tinnng. With tiny SMT parts you have to be careful about even small lumps of solder after pre-tinning or you will have coplanarity problems and possibly poor or no solder connections on some pins (that's the reason ENIG, gold flash or other non-HASL finish is usually used on boards with very fine pitch SMT parts). 

     

    If using flux, be sure to either use a no-clean flux or clean the board good or you'll have corrosion problems down the road.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Make sure you pretin the connectors and the board pad.

    when you add a little flux, you will get both ends of the solder to flow together more easily.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • camuyano
    camuyano over 10 years ago in reply to mlease

    Thanks, I like your idea. I do have some paste at hand. Will give it a try as soon as I can.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mlease
    mlease over 10 years ago in reply to camuyano

    Javier, get a small tube of solder past. Smear a little of the solder paste on the pins of the connector and then place it on the board. You do need a fairly fine pointed soldering iron tip but just place it each of the pin/pad joints to melt the solder paste. If you get a short between the pins, usually just running the iron tip between the pins will pull the excess solder away on the iron tip. Worst case use some thin solder wick to remove the short. It is unlikely you will remove enough solder to desolder the joint completely.

     

    That technique works rather well with fine pitch connectors and small ICs. Once you get it down it should only takes a few seconds per connector.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • camuyano
    camuyano over 10 years ago in reply to e14 Contributor

    I will take your recommendation and after a few more test will get a hold of a hot air gun to test it out. thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>