Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs PYNQ-Z2 Workshop - Session 1 blog 2
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: beacon_dave
  • Date Created: 28 May 2020 5:01 PM Date Created
  • Views 2024 views
  • Likes 7 likes
  • Comments 8 comments
  • pynq framework
  • pynq-z2
  • pynq workshop
  • pynqstarter
Related
Recommended

PYNQ-Z2 Workshop - Session 1 blog 2

beacon_dave
beacon_dave
28 May 2020

Continuing on from the previous PYNQ-Z2 Workshop - Session 1 blog,  this blog continues to investigate the topics covered in the Element 14 workshop session PYNQ-Z2 Workshop: Getting Started with PYNQ led by Adam Taylor, where we took an introductory look at the PYNQ-Z2 development board produced by the Tul Corporation.

 

Previously I had looked at using the logictools overlay and more specifically the Pattern Generator and Trace Analyzer in relation to a 4-bit gray code. This time I'm using it with the DMX512 protocol which is widely used for entertainment control purposes.

 

Once the PYNQ-Z2 development board is powered up and connected to the local network, we can use a web browser to log into Jupyter running on one of the microprocessor cores of the ZYNQ 7000 series device.

 

Here we create a new notebook and start interacting with the PYNQ framework.

 

First we download the logictools overlay supplied with the PYNQ-Z2 board image:

image

Then we create the WaveJSON waveform in WaveDrom mark-up:

image

In this instance we are creating a start frame plus 5 frames of data.

  • start frame is set to 0x00 to indicate dimmer frames
  • channel 1 is set to a value of 0
  • channel 2 is set to a value of 1
  • channel 3 is set to a value of 127
  • channel 4 is set to a value of 128
  • channel 5 is set to a value of 255

Annotations have been added to help illustrate the DMX512 format making use of the WaveDrom features.

  • m.a.l.c mark-after-last channel (minimum duration of 0s but only if at least 24 channels are present to comply with the minimum packet duration)
  • m.a.b mark-after-break (minimum duration of 88μs / two frames)
  • m.b.f mark-between-frames (minimum duration of 0, max of 1s)

The minimum permitted duration for a DMX512 packet is 1196μs, so this example would either need an additional 19 channels adding or alternatively an extended mark-after-last channel to pad out to 1196μs.

 

The 88μs break may also need extending to the recommended 100-200μs to accommodate receiver tolerances.

We can now display the waveform:

image

This is just the first 17 bits, the full 120 bits can be seen further down after the analysis has been captured and added.

 

We can now instantiate the pattern generator and trace analyzer objects to make use of this waveform data.

image

The analyser is set to capture 120 bits of data.

 

The pattern generator needs to be configured with the stimulus and analysis group wave names, the mode and the frequency.

By default the generator runs at 10MHz which is too fast for DMX512. Unfortunately its configurable range out of the box is 251.95kHz to 100MHz which is still slightly too fast for the 4μs pulses used in in DMX512, however not an issue with simulation, but would make the 88μs break too short to be recognised by some receivers.

The mode can be set to single shot or continuous looping. At this stage it is set to single shot, however looping will be required for a receiver test.

image

In order for the trace analyser to capture the pattern generator output, a jumper cable requires connecting between D0 and D19 on the Arduino interface to provide a loopback signal.

 

We can now run the pattern generator and trace analyzer and display both the generated (Tx) and captured (Rx) waveform:

image

image

image

image

image

image

image

After the capture we can stop the pattern generator:

image

 

As with the previous blog, this was fairly easy to configure and run. The Jupyter notebook environment is convenient to work with, and WaveDrom is quite flexible  once you get the hang of it.

 

Unfortunately the PYNQ documentation is a bit vague on how to use the logictools pattern generator with either of the PMOD (or the Raspberry Pi) interfaces as I have a PMOD RS-485 module sitting here eager to participate. It may have to be patched into the Arduino interface instead.

  • Sign in to reply

Top Comments

  • yuricts
    yuricts over 6 years ago in reply to beacon_dave +2
    Hi Dave, I have been digging in the docs, namely: In this source you see the TraceAnalyzers specification can be set (line 114-122): https://github.com/Xilinx/PYNQ/blob/master/boards/Pynq-Z2/base/base…
  • beacon_dave
    beacon_dave over 6 years ago +1
    adamtaylorcengfiet is there any information available on how to use the LogicTools Pattern Generator with either the PMOD or Raspberry Pi interfaces on the PYNQ-Z2 board ? ReadTheDocs keeps hinting that…
  • yuricts
    yuricts over 6 years ago in reply to yuricts +1
    I have been trying this, but I cannot find the correct pin mapping to the pmod. Feels like a dead-end... After reading Adam's blog here: https://www.hackster.io/news/pynq-edition-interfacing-with-pmods…
  • yuricts
    yuricts over 6 years ago in reply to yuricts

    I have been trying this, but I cannot find the correct pin mapping to the pmod. Feels like a dead-end...

     

    After reading Adam's blog here:

    https://www.hackster.io/news/pynq-edition-interfacing-with-pmods-arduino-and-raspberry-pi-61676f9f0fab

    It seems to be possible to write your own pmod driver, a bin file, which you can load, although it is being loaded from base, I don't see a way to do that with logictools...

     

    from pynq.overlays.base import BaseOverlay

    from pynq.lib import PynqMicroblaze

    base = BaseOverlay('base.bit')

    mb = PynqMicroblaze(base.iop1.mb_info, "/home/xilinx/pynq/lib/pmod/pmod_timer.bin")

    mb.reset()

     

    Here is some more information about the driver groups:

    https://pynq.readthedocs.io/en/v2.5.1/overlay_design_methodology/pynq_microblaze_subsystem.html

     

    The pmod_timer and pmod_pwm are the most interesting drivers in this case, the others all use i2c, spi, arduino...

     

    Another approach I am thinking of is to indeed see if we can change the SwitchIO IP block in the logictools project. It is not clear how to do that yet...

    You can open Vivado and source the tcl script logictools.tcl in in pynq/lib/logictools/ then you see the design of logictools... It is a big design... ctrl-f and search for io_switch... it is set to pmod... I expected it to be arduino? Confused...

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuricts
    yuricts over 6 years ago in reply to beacon_dave

    Hi Dave,

     

    I have been digging in the docs, namely:

    In this source you see the TraceAnalyzers specification can be set (line 114-122):

    https://github.com/Xilinx/PYNQ/blob/master/boards/Pynq-Z2/base/base.py

     

    https://pynq.readthedocs.io/en/v2.5.1/pynq_package/pynq.lib/pynq.lib.logictools.html#module-pynq.lib.logictools.pattern_…

     

    https://pynq.readthedocs.io/en/v2.5.1/_modules/pynq/lib/logictools/pattern_generator.html

     

    I am not sure yet, but I have the impression this might help:

    pattern_generator.intf_spec_name='PYNQZ2_PMODA_SPECIFICATION'

     

    What do you think?

     

    Kind regards,

    Yuri

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago

    adamtaylorcengfiet is there any information available on how to use the LogicTools Pattern Generator with either the PMOD or Raspberry Pi interfaces on the PYNQ-Z2 board ?

     

    ReadTheDocs keeps hinting that it can be done, but also appears to contradict itself in places (probably due to the interface differences between the Z1 & Z2), and that it is even automatic via the Interface Switch assuming that you supply the correct pin names but they don't appear to be documented ?

     

    Even if it can't directly connect to the PMOD IOP then presumably the LCP for the Raspberry Pi should be able to access  the PMODA interface which is shared with 8 pins of the RPi header ? However I can't find any examples of how to use the RPi interface with the Pattern Generator either.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<