Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gene Breniman's Blog Continuing to organize - building a tool holder...
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 23 Jan 2021 11:13 PM Date Created
  • Views 2001 views
  • Likes 11 likes
  • Comments 16 comments
Related
Recommended

Continuing to organize - building a tool holder...

genebren
genebren
23 Jan 2021

In my prior blog (Starting the New Year with a clean up and reorganization ..... ) I started work on organizing my office workspace.  Today I finished building a tool holder for my Soldering/Building workspace within my office.  I saw a nice looking, 3 tiered tool holder online, but thought "Hey I could build that" which then morphed into "Yeah, I could even make it better at the same time".  In stead of a free-standing block, I could build my tool stand to span the width of a shelve in the shelving unit over my soldering/building station. So I took some measurements and sketched up a super rough plan and then when out to the shop to see what I could come up with.

 

imageimage

I started with a couple of cut ends from some cedar 2"x4"s that I had in the shop.  I then ripped one of them down to 2"x2 1/2".  Next I ran them both through the planer a couple of times until they were both smooth and true, and the thickness of the boards were 1 1/4".  Next I drilled hole into the two pieces, 3/8" holes, 1" apart in the back piece and alternating 1/2" and 3/4" holes, 1 1/2" apart in the front piece.  The holes are flat bottomed and a drilled down to within 1/2" of the bottom edge of the boards.  I then drilled/cut and sanded notches into the ends of the boards that would eventually clamp to the shelving unit uprights (~3/4" tubing).  The final drill operation was to drill through the two pieces for the two quick change bolts that will be used to clamp the two pieces together.

 

After test fitting everything back in the office, I returned to the shop to finish the pieces.  I did a through sanding on the two pieces and then applied a weathered gray stain to the boards.  After the stain dried, I apply two coats of a satin water based varnish finish.

 

Today, after the finish was dried, I installed the tool holder.  Here are some pictures of the tool holder in place:

 

image

imageimage

I will be trying this out for a couple of day to see if I need any modifications or adjustments to the installation.  I have some other organizers and tools on order as I still feel I could add a few more improvements.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 5 years ago in reply to fmilburn +4
    Thanks Frank! I had a lot of fun building it and hopefully it will assist in keeping things organized.
  • fmilburn
    fmilburn over 5 years ago +3
    Oooh, nice
  • Andrew J
    Andrew J over 5 years ago +3
    Swent. Home built solutions are so much more satisfying.
  • genebren
    genebren over 5 years ago in reply to shabaz

    Thanks shabaz.  I used T-bolts, with a routed (chiseled) slot around the back side, around the hole, to hold the bolt captive.  I 'borrowed' the t-bolt and the knob, from a pair of my router clamps (spares).  Here is a picture:

    image

    These clamps are intended to work with aluminum T-rails.  I though I had a bunch of these t-bolts and knobs somewhere in my collection of parts, but I was not able to find them.  Fortunately I did have a pair of clamps left over that I could use until I find the extras.

     

    The hammered in nuts are called 'Tee Nuts', 'Tee Pronged Nuts' or 'Blind Nuts'.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago

    Hi Gene,

     

    That looks great! Very clever design. Are you using the hammer-in nuts (I forget what they are called) on the other side?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago in reply to dubbie

    Thanks Dubbie. I have tended to use drawers to mange my tools, but lately I have found that tools piled into drawers still have the potential to have 'lost' tools.  I also find that I tend to sweep tools and other junk into the drawers when I need to clean up space, only moving the mess to be dealt with later.  The open and visible storage might help, only time will tell.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago

    Gene,

     

    Very neat. I hadn't thought of organising my tools. I currently keep them in a small pile near my right hand. Sometimes one disappear for a while but eventually it will re-appear. Maybe some sort of desk top box tool=holder might be a good idea. Maybe even a mug might work.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to genebren

    I don't know what happens with the editor on this site.  It either capitalises the second word, or garbles it into rubbish - either way, I always have to go back and adjust word two in a post.  I have no idea what swent is, but meant sweet!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>