Personal Blogs
  • Community Hub
  • More
Personal Blogs
Gough Lui's Blog 433Mhz Reverse Engineering Part 2 - Burning Questions are Answered
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 13 Apr 2016 10:00 AM Date Created
  • Views 1633 views
  • Likes 3 likes
  • Comments 7 comments
  • ook
  • 433.92mhz
  • security
  • remote control
  • radio
  • 433
  • remote
Related
Recommended

433Mhz Reverse Engineering Part 2 - Burning Questions are Answered

Gough Lui
Gough Lui
13 Apr 2016

I couldn't help but wonder, based on the previous posting and the discussion, exactly how did the 1 million combinations come about? Also, what are the functions of the fixed bits? Are they fixed pre-amble as my experience would suggest? Are there more hidden channels in the equipment than are used by the senders and that I know of? Can it cope with over-speed transmissions, shortened repetition delay times, less repetitions?

 

I embarked on a journey of "knowledge" by building myself a generic 433Mhz ASK/OOK transmitter that took a string of the following variables:

zero pre-low (us), zero high (us), zero low (us), one pre-low (us), one high (us), one low (us), delay (us), repetitions, data

 

I figured that, by using these timing variables, almost all my ASK/OOK fixed code protocols can be represented, thus a serial to ASK/OOK "universal" bridge was born. This was used to probe the switches and find the truth.

 

The answers are in my blog post at http://goughlui.com/2016/04/13/reverse-eng-pt-2-watts-clever-easy-off-wsmart-box-es-aus1103/

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago in reply to Gough Lui +1
    I never tried the 'fixed' bits as there were plenty available for the purpose. It was found that bit 25 , namely the last fixed bit, appears to be a do-not-care bit. No matter whether it is 0 or 1, regardless…
  • mcb1
    mcb1 over 10 years ago in reply to Gough Lui +1
    I'm guessing it wasn't entirely inexpensive? No it wasn't. Not sure if it was old stock when we brought it way up at Coloundra a few years back. Looks like they might have these http://www.bunnings.com…
  • mcb1
    mcb1 over 10 years ago in reply to mcb1 +1
    A little more searching found these useful links Reverse engineering the RF protocol on a Kambrook Power Point Controller - BeyondLogic Kambrook Remote Power Outlet & Arduino - working https://discuss…
  • mcb1
    mcb1 over 10 years ago in reply to Gough Lui

    I never tried the 'fixed' bits as there were plenty available for the purpose.

     

    It was found that bit 25, namely the last fixed bit, appears to be a do-not-care bit. No matter whether it is 0 or 1, regardless of what it was when learnt, the command will be executed.

    I wonder if the devices are actually two channels, with the last bit used for the night light.

    If you check the spreadsheet you'll see that the light uses bit 24 on the ones I had.

     

     

    I picked up a Kambrook version of these on your side of the ditch.

    It had 4 banks, but since they weren't available here (even though Bunnings is) I never tried 'hacking' it.

    image

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago

    mcb1, as usual, I have to thank you for your spreadsheet that put these thoughts into my head and made me try and find out what the fixed bits actually mean.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<