Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips - Bread Board Alligator Clips
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 2 Sep 2019 3:32 AM Date Created
  • Views 5033 views
  • Likes 11 likes
  • Comments 19 comments
  • bread_board_cables
  • shop_tips
Related
Recommended

Shop Tips - Bread Board Alligator Clips

jw0752
jw0752
2 Sep 2019

Recently I was working on a bread board circuit provided by jc2048 . One of the things that I find very convenient when wiring up a bread board are short wires with an alligator clip on one end and a bread board pin on the other. I use these cables to hook up peripheral meters, sensors, and actuators to the bread board circuit. In the past I have taken cheap alligator to alligator jumper cables, cut them in half and just added a bread board pin to the cut end. While this works the cables do not turn out to be long term durable or dependable. For one thing the wires of these cables are seldom soldered to the alligator clip. Instead the copper wire (what little there is) is folded back alongside the outer insulation and then the alligator clip is crimped down on the wire and the insulation. I have taken brand new jumper cable made like this and had resistance readings of 1 Ohm from alligator to alligator.

 

After fighting with my old patch wires on this last bread board I decided to take the time and make up some that would be of better quality and more durable. I began the project with a bag of the same old cheap jumper cables.

 

image

 

This would be the source of Alligator clips and covers for the new Bread Board Clips. I will be using special wire that I have salvaged from dental handpiece cords for the wire in the new BB patch cables. This wires has an overall small diameter but has an over sized multi strand conductor. One day I took the time to count the strands on one of these type of wires and there was over a hundred strands. This many strands makes the wire very flexible and the over all gauge allows the wire to carry a reasonable current. In the dental application this type of wire will often carry 2 or 3 amps. Here is a picture of the original jumper cable wire along side one of the special wires.

 

image

 

The alligator clips that I had salvaged from the cheap jumper cables were next soldered to the high strand wire and the crimp at the back of the alligator clip was used as intended to provide a strain relief on the wire. As much as possible I try to use matching colors in the construction of the BB clips. At 70 there are enough things to confuse me when I build without any color confusion.

 

For the pin end of the cables I will take standard square pin, breakable, male headers and add them to the free end of the wire. The solder is covered with a short piece of heat shrink which serves as an insulator and also a strain relief so that the wire is not stressed at the solder joint.

 

Here is what the bag of jumper cables has turned into:

 

   imageimage

 

With the new alligator patch cables in hand I set up the experiment that had inspired me to make them.

 

image

 

The flexibility of the cables make it easy to set up and position. My old cables were constantly applying torque to the circuit board in one direction or another making it difficult to get things to stay where I wanted them. The net out of pocket cost of this project was under $3.

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +8
    Hi John, They look great! I have soldered the alligator clips to the wire that comes with them in the past, but it really is poor quality wire. Do you find this approach for the pin end: For the pin end…
  • dougw
    dougw over 7 years ago +7
    Great idea John. One thing I find frustrating is how slippery some of those sleeves are on the alligator clips. It is hard to get your fingers squeezing in the right direction on some of them. I have some…
  • Gough Lui
    Gough Lui over 7 years ago +6
    Doing some searching on element14 - it seems it is possible to buy such wire in the Hook-Up wire section. One just has to be careful to filter by gauge and strand counts to find something decently flexible…
  • balearicdynamics
    balearicdynamics over 7 years ago

    John, I am still using your hand-made tester terminals and are still are an incredibly great solution in so many situations. Also, this idea in its simplicity sounds great. I have also the need you illustrate and making this kind of gator-to-clip makes really easy to testing and checking, especially on custom boards not easy to associate directly to a breadboard. I have always used double alligator cables but this is definitely a better solution.

     

    Enrico

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to jw0752

    I worked with a multi-crew installation team. Among other electronic projects we installed electronic systems in air traffic control towers. Gray tubs rolled of the truck with everything from wire to components. Keeping stock of two different colours of heat shrink tubing was a chore in itself. Your OCD would have had you twitching in our environment.

     

    You can only travel with so much stuff. After that it gets cumbersome to transport and maintain. Unfortunately that seventeen year career laid the foundation for my shop today. IC sockets can make ideal test and connection points, especially when in develop when you don't know what you don't know.

     

    Sean

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to colporteur

    Hi Sean,

     

    Being a little OCD is good for something.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 7 years ago

    Your experience with the quality of alligator clip jumpers usually rears it ugly head while troubleshooting a dog fault. An intermittent faults that doesn't stick around long enough to get a handle on the root cause. After a few attempts at isolation you discover an open in a jumper cable. FK!!!!!!!!! Fart kickers.........

     

    I'm in impressed with your supply shelf that has both the wire colour selection and matching colours for heat shrink. NICE:)

     

    Sean

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago

    Another great tip for working better!

     

    I do make a lot of use of various sizes of micro-grabbers. Smaller ones are quite cheap and I find easier to manipulate. The larger ones get more expensive but then I do not need so many of them.

     

    Example Micro-grabbers

     

    Kind regards.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
>