Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips - Bread Board Voltmeter
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 5 Nov 2015 7:17 AM Date Created
  • Views 1033 views
  • Likes 3 likes
  • Comments 10 comments
  • voltmeter
  • shop_tips
  • bread_board_meter
Related
Recommended

Shop Tips - Bread Board Voltmeter

jw0752
jw0752
5 Nov 2015

There are many times, when I am working on an experiment or project using my bread board, that I want to monitor the voltage at different points in the circuit. This usually involves setting up a couple DVMs and running test clips into the proper positions on the board. This can be messy and inconvenient. I got the inspiration for this shop tip when I saw these small 2.5 volt to 30 volt LED meters on a China Dollar Store site for $2.75 each, including shipping to the shop.


image


I bought two of the little meters and added some bread board pins onto the wires.


image


The next step was to calibrate them against my Fluke which is perhaps the most accurate meter in my shop. I calibrated them around 15 volts as I am sure they are not completely linear and this at least centers their range. Surprisingly they stayed within 0.1 volts of the Fluke throughout the range. Since the meters were very light I wanted to mount them to a more substantial base. I cut some small pieces of wood and mounted the boards and also a tilt prop to the back of the boards.


image


image


image


It is important to note that these meters consume about 20 mA at all voltages above 5 volts. This could be a factor and affect our experiment if we are not careful. I have labeled the meters with this information so that I am careful to only use them in positions where their current draw will not affect my circuit or the outcome of my experiment. If I need a voltage reading where minimal loading is required I will have to go back to the old method and hook up one of the DVMs.


For the sake of illustration I have bread boarded an LM7805 and used the two new bread board meters to monitor the input and output voltage of the regulator.



image



John

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +1
    Excellent idea. I have some of these up at the Ski field to show the voltage ...no more surprises now when the alternator isn't working.\ I intend to put one on the battery in the caravan but I'll be adding…
  • Problemchild
    Problemchild over 10 years ago +1
    Good one John, I've started doing the same thing after I saw someone doing a demo at a meeting doing the same thing. He was using it to remind himself that it was 5V not 3.3V to prevent him blowing the…
  • dougw
    dougw over 10 years ago +1
    Cute idea. You can get very similar modules with 3 wires, allowing the power to be separate from the signal, so you can measure from 0 to 100 volts. Doug
  • Problemchild
    Problemchild over 10 years ago in reply to jw0752

    Im doing a new revision of that board I'll mention this to  shabaz no doubt we'll see a load of these in use soon image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to Problemchild

    Thanks John,

    If you make one I think it would look better on one of your plexiglass creation stands. I would have preferred plexiglass but I seem to have better luck with wood.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to mcb1

    Thanks Mark,

    I believe that one of the first time I saw one of these in use was when you did your post on the ski field.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to jw0752

    Hi John,

     

    Here is the web address:

     

    http://www.repairfaq.org/sam/sambook.htm

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to DAB

    HI DAB,

    I thought about making an ammeter too but I will have to go to the 3 wire variety to do this as this 2 wire will only read down to 2.5 volts since the LED display is powered off the potential being measured. Any kind of a reasonable shunt would pull the voltage below the 2.5 volt minimum. I will probably make a 3 wire one up as you are correct a current meter would also be handy.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>