Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Flight Simulator 101 or back to college - part 16: C Structures with in Structures
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 3 May 2023 5:34 PM Date Created
  • Views 1553 views
  • Likes 9 likes
  • Comments 12 comments
  • flight simulator
  • nexgen
  • back to college
  • c programing
  • flight simulation 101
  • data structures
  • struct as member of a struct
Related
Recommended

Flight Simulator 101 or back to college - part 16: C Structures with in Structures

phoenixcomm
phoenixcomm
3 May 2023

imageNow, Somewhere on the Stack Exchange, I heard some crud about you just can't have a struct as a member of a struct. Well, you sure can and now for all the curious minds out there I will show you how to do it. Remember I work with flight simulation, so you always need to know where you are. This is called position, and it is made up of both a Latitude and a Longitude which are both structures of themselves, enclosed in an outer structure. 

First I need to create two structs called Lat and Lon and I will make them out of a structure that I call DM, or Degrees and Minutes, and you also need to know the Hemisphere or hemi. 

struct DM {
	int degrees;
	float minutes;
	char hemi; 
	};

struct DM Lat;
struct DM Lon;
Now that I have that out of the way, I need to put this                   together and create my three structures: Current, Start, and Finish. You will note they all have a             structure type of Position. So you ask how do I access them? Well, you just use dotted notation.

struct Position{
	struct DM Lat;
	struct DM Lon; } Current, Start, Finish;
// Carswell: 32-46.151167N 097-26.492083W
	Start.Lon.degrees  = 32;
	Start.Lon.minutes  = 46.151167;
	Start.Lon.hemi     = 'N';
	Start.Lat.degrees  = 97;
	Start.Lat.minutes  = 26.492083;
	Start.Lat.hemi     = 'W';

Now, I hope I have helped some of you.. I think this will close this blog.  

  • Sign in to reply
  • colporteur
    colporteur over 2 years ago

    You make it looks so easy:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dang74
    dang74 over 2 years ago

    I wasn't aware of this restriction but when you Google you do indeed see some results indicating that you can't have a struct as a member of a struct.  At any rate, I'm glad you smashed through this 'barrier'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<