Polls How do you plan out your electronics?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 19 Jun 2020 1:00 PM Date Created
  • Last Updated Last Updated: 19 Jun 2020 1:30 PM
  • Views 1983 views
  • Likes 1 like
  • Comments 32 comments
Related
Recommended

How do you plan out your electronics?

I realise that I perhaps don't prototype how I should. Often some of the components are plug and play, or I just rebuild the circuit every time with a breadboard, but with my larger projects I've realised that I do need to document them in some manner else when I have to rip them apart and come back to them... I'm not sure how it went together, so what do you do?

 

This poll is featured in Round-Up and Review - Videos, News and Polls!

  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 6 years ago +6
    I wanted to tick three boxes, Simulation, draw a proper diagram, design the pcb. You didn't provide a simulation box, which is a shame since this is (or should be) a key part of analogue design. Occasionally…
  • jc2048
    jc2048 over 6 years ago +6
    Paper and pen. As an example, this was the plan of a layout [bird's nest style, not pcb] for Frank's op amp that I showed in the comments to his blog here Op-amp made from Discrete Components
  • colporteur
    colporteur over 6 years ago in reply to michaelkellett +6
    Your technique of relaxing has worked for me in the past. I find coupled with a good sleep and by good I mean, a few restful nights that the bladder doesn't have to use the white phone every three hours…
  • shabaz
    shabaz over 6 years ago in reply to Fred27

    I like reading up as much as possible before starting a project. However, I wish I did that in other areas too. Also the actual work part of it reminds me of Agile. I should have used it for woodwork!

    I spent several weeks (on and off) doing a seat-of-the-pants woodwork bit of fun project, using whatever I had in the shed, to make a bar-stool that converts into a table, and also as a book-tidy. It was to be a masterpiece 3-in-1 bit of furniture : )

     

    I had no plan though, and didn't really design and test anything, so it was ad-hoc bits of thought as I went along with the construction.

    However the reality was not great! I had not considered how the leaves would work.. since they don't fully fold and just hang down, in practice if anyone sits on it in the bar-stool mode, then the legs tend to press against the hinge edge of the leaf.. think it will cause the hinges to pull off over time : (

    I should have prototyped up the bits I was unsure of, before getting too far in the construction : ( As it is, I cannot back out now, so the project has this fundamental flaw forever : (

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago in reply to dubbie

    That's the big difference between a hobby and a job. With a hobby, the end goal is to enjoy the process and perhaps learn along the way. There's nothing wrong with abandoning a project, parking it because something more interesting came along, using the "wrong" tool because you wanted to learn to use that tool, etc. Your only deliverable is that you had fun in your free time. Of course, some of the fun is to be proud of something you finished too. image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    I seem to be in a majority of just making it up as I go along. I just like the creative feeling of this approach. Usually a bottom up design approach as well, start with the Nano and work outwards. I just enjoy the crazy freedom of it all. I used to have to be organised and on-time when I was working which I may now be rebelling against, so I really enjoy to just do whatever I feel like whenever I feel like it approach I now use. I don't always finish and it doesn't always work but I don't care, I just enjoy the process.

     

    I have started trying to make 3D printed coverings for the projects I'm making now, which has restricted my chaos, but I enjoy the process of design to reality of the 3D printer. I use TinkerCAD and it can be used in the bottom up make-it-up -as-you-go-along method I like. One day, I might even get it right.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago

    I normally prototype to test the concept with dev boards where possible and then it's straight to Eagle.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sean_Miller
    Sean_Miller over 6 years ago

    I start with Eagle and Autodesk Fusion 360.

     

    After those look pretty when rendered, I breadboard to make sure I didn’t miss anything. 

     

    Then I go to oshpark.com with the .brd and have the board in a set of three delivered two weeks later.

     

    sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 6 years ago

    Wing it.  Okay. so I do start with a schematic - but it could be on a series of Post-it notes.  It might get breadboarded and it might go straight to protoboard.  Someday, I'll get serious and use the copy of Eagle I bought and make a genuine PCB.  THEN I will probably have a less haphazard process.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago

    I draw a schematic by hand or with KiCad.  My silly mistakes are greatly reduced by doing so. If it is complicated and I am still sorting my thoughts I will start with a block diagram.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago

    Proper diagrams, incremental (baby steps at a time). Usually pencil and paper.

    CAD if I plan to make a PCB.

    I just picked up simulation - trying out Tina-TI and LTspice. The recent discussions here on opamps were helpful to get hands dirty.  

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aswinvenu
    aswinvenu over 6 years ago

    I generally start with the schematics. Break down the analog and digital parts.

    Do simulations if simulations are required on the analog side.

    Make a prototype. This depends on the complexity of the project.

    If its not containing many analog components, Then I will prefer breadboards

    and development boards for prototyping.

    If the project is complex and has more analog design then I will design the PCB

    and go get the prototypes made from a local vendor.

    Mean time i will write the board bring-up softwares/firmwares.

    Then testing and validation of hardware.

    At last if I am satisfied with the product then final release else another iteration of the design steps.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 6 years ago

    I usually start by designing schematics and PCB layouts on CAD. I don't use simulation although I do all calculations necessary to ensure the circuit will work.

    I almost always design a PCB to build a prototype,  although I will use strip board if I don't have time to order a PCB and occasionally might use a breadboard to do a quick proof of concept or allow software testing before the PCB shows up.

    I have so many extra PCBs lying around (because I always print more than I intend to populate) that I can sometimes find one that can be re-purposed. This works because I usually build in extra features on every PCB beyond what is required for the current project.

    Actually the start of the process is just meticulous visualization in my head, which gets augmented by research before I start the tangible design process.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>