Arduino
  • Products & Partners
  • More
Arduino
Blog Self Balancing Robot - Temporary Diversion from the Quadcopter Project - Demo
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ipv1
  • Date Created: 15 Apr 2015 4:37 AM Date Created
  • Views 3251 views
  • Likes 7 likes
  • Comments 11 comments
  • robot
  • ip_iot
  • arduino
Related
Recommended

Self Balancing Robot - Temporary Diversion from the Quadcopter Project - Demo

ipv1
ipv1
15 Apr 2015

Abstract

As most of you know, I am doing a quadcopter from scratch project where I make almost everything from scratch. In doing so, I had to understand the dynamics behind the software/firmware and in order to explain the quadcopter, I can start by explaining a balancing robot. In this post, I explain the build and provide a video demo for the robot. Lets go!

 

The build

I usually build stuff from scrap and recycle what I can and this project is no different. I start with some scrap wood and made a simple box like frame. I trimmed off wood from the sides to reduce weight and to make it a little more presentable. Finally I added some paint and a quick and dirty job later, I have a robot frame.

IMG_20150411_201416.jpg

As you can see, in the above pic, I have some motors and wheels attached as well. I bought the wheels a long time back and the motors were purchased online. These motors are 288RPM 12V rated and have optical encoders so that we can track the distance moved by each wheel. I clamped these motors in place using some sheet metal pieces I cut up from the scrap tin boxes I had. You can use soft-drink Tins etc as a source of the sheet metal and self threading screws to attach them to the wooden base.

 

In order to drive the motors, I am using an L293D motor driver which came from an older robot which lost it's wheels in an accident. image

Since we need a place to put the control board, I used a cardboard box and cut out an H shaped plane to sit atop the motor driver floor. The control board itself if an Arduino Uno which I received as a part of the Internet Of Holiday Lights Challenge from Element14 and I made a shield for the MPU9150 breakout board. The image below shows the same shield but on the FRDM K64F board which I was using for the quadcopter.

IMG_9611.jpg

I scraped together some libraries from the internet for the MPU9150 as well as PID control and a few hours of head scratching later, it actually worked! The video below shows the working robot in action.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I had some failures along the way but it was quite easy and only a few hours of work once you know what you are doing. In the next post, I will be sharing some more details on the code as well as things that you need to consider when making one yourself.

 

Cheers,

IP

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 11 years ago in reply to 4ringfan +3
    Mark Sir, Thank you. I am writing a detailed article/blogpost/roadtest review for the FRDM K64F which uses onboard sensors and replaces the arduino. It will be posted in the Freedom/ARM sections in the…
  • mcb1
    mcb1 over 11 years ago in reply to ipv1 +3
    IP/Mike It is easier to balance a broom with the heavy end at the top. You are quite right that the tipping movement becomes greater and occurs faster ith the weight up high. David Anderson made one called…
  • dtsartsanis
    dtsartsanis over 11 years ago +2
    Very interesting project.
  • jw0752
    jw0752 over 11 years ago

    Hi Inderpreet,

    Very cool. I like how you use salvage and common parts to make the self balancing robot. I look forward to reading more about this project. This last week I salvaged out a Kodak Printer and ended up with a couple nice motors with optical encoders. I have been studying the motors with the hopes of interfacing them and controlling them with the arduino. Hopefully I can learn something from your posts.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<