Arduino
  • Products
  • More
Arduino
Blog Sleepy Blink
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 10 Jul 2016 11:20 AM Date Created
  • Views 1614 views
  • Likes 4 likes
  • Comments 6 comments
  • arduino uno
  • 4tronix
Related
Recommended

Sleepy Blink

Workshopshed
Workshopshed
10 Jul 2016

I've been given a new board from 4tronix to RoadTest, which is compatible with an Arduino UNO but with a significantly different form factor. The board is still in beta so has yet to gain a proper name.

image

The board is 27mm in diameter about the same size as a£2 coin it has a ATMega328P-AU microcontroller and a CH340G USB interface A blue LED is attached to pin 13 4 digital and 4 analogue pins are broken out along each size with the power connectors top and bottom

 

On the back of the board is a rechargeable Lithium ION coin cell which 4tronix thought should have a run time of about 1 hour. There is a small power switch so you can turn it off to save the battery or to speed up charging.

 

My first thought was to see if we could increase that with some power management. So I created the following "sleepyblink" code which flashes the LED for just 100ms before sleeping for 1s. The board uploads quickly, although I did see that the board changed COM port number when I powered it off an on which might cause irritation when programming it.

 

 

//Library from http://www.rocketscream.com/blog/2011/07/04/lightweight-low-power-arduino-library/#sthash.PhJ0PF9f.dpuf
#include "LowPower.h"
int ledPin = 13;                 // LED connected to pin 13
void setup()
{
  pinMode(ledPin, OUTPUT);      // sets the digital pin as output
  delay(5000);                 // Nice long delay to help with reprogramming    
}
void loop()
{
  digitalWrite(ledPin, HIGH);    // sets the LED off
  delay(100);
  digitalWrite(ledPin, LOW);   // sets the LED on
  //Sleep
  LowPower.powerDown(SLEEP_1S, ADC_OFF, BOD_OFF);
}

 

The battery lasted over 33hrs, it stopped over night whilst I was asleep so I know it was less than 41hrs.

 

Next up is to make a simple badge.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to Workshopshed +1
    As long as the SLEEP_MODE_PWR_DOWN is used, it should be the same. That is the maximum sleep mode. The Timers and so will be turned off, but an output pin keeps its output level. Perhaps the CH340G is…
  • beacon_dave
    beacon_dave over 10 years ago in reply to Workshopshed +1
    Atmel have an application note on reducing power consumption which may be of interest. AVR4013: picoPower Basics http://www.atmel.com/Images/doc8349.pdf There is also some related content on the Atmel…
  • DAB
    DAB over 10 years ago

    Looks like an interesting board for small projects.

     

    You should be able to use some basic power management techniques to get long life from you batteries.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<