Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69862 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
  • sciguy14
    sciguy14 over 15 years ago in reply to dirtdiver

    Use a delay() function to slow it down.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi, i am currently trying to connect wishield 2.0 (http://www.asynclabs.com/store?page=shop.product_details&product_id=26&category_id=6&vmcchk=1) with my arduino mega board.My idea was to control my RC plane with I-phone. But I am not sure how to connect wishield and arduino mega. Can you tell me how to do step by step? thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    It use's SPI communication.  The Wishield Library includes info and examples of usage: http://www.asynclabs.com/wiki/index.php?title=WiShield_library

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 15 years ago in reply to sciguy14

    Regarding the creation of a Wiegand output, I stumbled across this tutorial: http://arduino.cc/en/Tutorial/SecretsOfArduinoPWM and within this tutorial an additional example and manual creation of PWM: http://www.arduino.cc/playground/Main/PWMallPins

     

    The tutorial describes different methods of manipulating the PWM duty cycle which to me, sounds as if you could use two output pins to create a Wiegand output directly with Arduino rather than a C library. The question is which method would be best, namely:

     

    Simple Pulse Width Modulation with analogWrite
    Bit-banging Pulse Width Modulation
    Using the ATmega PWM registers directly
    The Atmega 168/328 timers.
    Fast PWM Mode
    Phase-Correct PWM
     
    Or if none of these would work, I would be curious to learn why.
     
    Your help is greatly appreciated.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to BigG

    You can't say which is "best" without an application in mind.  Each will have their merits, but I'm sure only one is the ideal solution in a particular scenario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 15 years ago in reply to BigG

    Hi BigG,

     

    Since you appear to be knowledgable about both forms of wave generation, why don't you do some experiments and share the data?  Maybe we can assess the merits of both on some test applications and give the whole group some useful data.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to DAB

    Hi, I change in my arduino chip, befor use atmega 328, now I put in socket atmega8 16PU, and dont work he, what is problem.

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • leon_heller
    leon_heller over 15 years ago in reply to e14 Contributor

    You need a 328 chip with the correct Arduino bootloader.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WestfW
    WestfW over 15 years ago in reply to leon_heller

    Currently the Arduino "system" supports ATmega328, ATmega168, and ATmega8 chips.  It does have to have a bootloader pre-installed, and you have to select an appropriate "board" in the tools menu.  If you put an Atmega8 in an Arduino Uno board, you should tell the IDE that you have an "NG or older with atmega8" (the "board type" has more to do with the chip and the  bootloader than it has to do with the rest of the board.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi, im new to arduino but im doing a project whereby i want to control a 3 digit seven-segment display with 74HC595 shift register and with an analog keypad input. how do i do the code because i have tried and nothing appears happens. im confident of my connection but sometimes my arduino has problems, it can't be detected by my computer and that has let to a few problems with uploading the code to the board so sometimes i get confused when my ardunio has problems or if the code is not the right one for my seven-segment. Can you help me with this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>