Arduino
  • Products
  • More
Arduino
Arduino Forum Question on a part I need
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 418 subscribers
  • Views 1340 views
  • Users 0 members are here
Related

Question on a part I need

e14 Contributor
e14 Contributor over 15 years ago

I need a rotating control to adjust some LEDs.

 

However I would like it to infinitely turn (unlike a potentiometer).

 

This is the sort of thing you would get as a volume control on an AV amplifier.

 

Any help on what they are called and links would be great.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to tronixstuff

    I wondered about that but Im getting random results so on a forward movment I could be 3 forward and one back or 1 forward and one back ect.

     

    Interestingly I also tried this code:

     

    http://www.arduino.cc/playground/Main/RotaryEncoders

     

    But I just get an incrementing number even when I dont touch the encoder at all.  image

     

    I have not had a lot of time to look at it so I am sure its not hard but will try to make some time today or tomorrow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 14 years ago in reply to e14 Contributor

    I will offer some thoughts for T.O.M. and others in hopes that some may find them useful in their search for enlightenment.  This problem sounds like the classic debounce dilema.  What does the digital pin on the arduino expect on its input?  Remember that the pin can be configured in one of three ways.  The choices are current source OR current drain (for output mode) OR Tri-state (Hi-Z).  External to the pin we can attach either a pull down OR a pull up resistor if needed.  The Channel A and B switches are configured to either connect the digital input pin to Vcc or Ground as is appropriate.  I will take a leap of faith and say that in all probability the center pin C is a common  to be connected to the correct level of signal voltage.  The encoder data sheet states the the maximum current the switches are rated for is 1 mA @ 5 VDC.  Therefore,  5 V / 1 mA = 5 k ohms or larger resistors are required to be placed in series with the switches to limit the current to achieve the designed life of the pico-switches inside this encoder.  This begs the question: "How many mA are required to allow the digital pin to recognize that there is now a logic ZERO signal on the pin?"  Hmm . . . oh wait . . . Doesn't "low-power CMOS" sort of necessarily imply very low current requirements!

     

    On page 76 of the ATmega328p data sheet it states: "If PORTxn is written logic one when the pin is configured as an input pin, the (internal) pull-up resistor is activated."  So depending on what the Arduino Team chose (current source or Tri-State) in the implementation of input mode on digital pins; there may not be a requirement for an external pull up resistor AND the encoder's common pin should simply be connected to ground to function without bouncing excessively.  If the signal is erratic then there is a good chance that the pull up resistor is a requirement.

     

    -=Syntax Matters=-

     

    Post Script:  Revealed on page 93 of Simon Monk's Programming Arduino GSWS book that the internal pull-up resistor is not enabled unless and until the following lines of code are executed:

    int inPin = 5;

    pinMode(inPin, INPUT);

    digitalWrite(inPin, HIGH);

     

    //(Alternative Option)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<