Arduino
  • Products
  • More
Arduino
Arduino Forum Controlling stepper direction with a button
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 419 subscribers
  • Views 3154 views
  • Users 0 members are here
Related

Controlling stepper direction with a button

e14 Contributor
e14 Contributor over 13 years ago

I am trying to control a unipolar stepper with two buttons, one on either side of a salvaged typwriter cage. The sketch will run it one one direction but the

button does not reverse the motor. Thanks for advise.

 

#include <Stepper.h>

Stepper s(20,8,9,10,11);

int button1 = 1;

int button2 = 2;

int buttonState1 = 0;

int buttonState2 = 0;

 

 

void setup()

{

pinMode(1,INPUT); //buttons

pinMode(2,INPUT);

 

pinMode(8,OUTPUT);

pinMode(9,OUTPUT);

pinMode(10,OUTPUT);

pinMode(11,OUTPUT);

 

 

s.setSpeed(500);

s.step(1500); // This is well beyond the max range but I assumed that when the carriage hit the button, it would reverse.   

//delay(5000);

}

 

 

void loop()

{

buttonState1 = digitalRead(button1);

buttonState2 = digitalRead(button2);

 

 

if (buttonState1 == HIGH)

{

s.setSpeed(-500);

s.step(1500);//200

//delay(1000);

}

 

 

if (buttonState2 == HIGH)

{

s.setSpeed(500);

s.step(-1500);

delay(1000);

}

 

 

 

 

}

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Blacksheep32

        This sketch "works" sometimes, but then has a mind of its own! The button input is not responding quickly and is a little sluggish.

     

    #include <Stepper.h>

     

     

      int button1 = 2;

      int button2 = 3;

      int stepCount=0;

      int buttonState1 = 0;

      int buttonState2 = 0;

      const int stepsPerRevolution = 100;

     

     

      Stepper myStepper(stepsPerRevolution, 8,9,10,11);          

     

     

    void setup() {

     

     

      Serial.begin(9600);

      pinMode (button1,INPUT);               //shift to pin 2

      pinMode (button2,INPUT);               //shift to pin 3

      myStepper.setSpeed(30);

     

     

      myStepper.step(1);

      //delay(500);

      digitalWrite (button1, LOW);

      digitalWrite (button2, LOW);

    }

     

     

    void loop() {

      buttonState1 = digitalRead (button1);

      buttonState2 = digitalRead (button2);

     

     

      if (buttonState1 == HIGH)

      {

      stepCount ++;

      }

      if (stepCount >1)

      {               

      myStepper.step(stepsPerRevolution);//stepsPerRevolution

      }

      if (buttonState2 == HIGH)

      {

        stepCount --;

      }

      if (stepCount  < 1)

      {          

      myStepper.step(-stepsPerRevolution);

      }

      Serial.println(stepCount);

    }

     

     


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark,

        This sketch "works" sometimes, but then has a mind of its own! The

    button input is not responding quickly and is a little sluggish.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Sorry Keith

     

    I've been tied up with something else, that had to get done.

     

    Apologies the sketch I posted, I forgot to change the 'int button' to the new pins, but I see above you've corrected that.

     

    If I understand correctly the stepper library will go away and do its thing, and come back when its finished.

     

    Imagine sending 'someone' down the road to the corner.

    If you want to tell them to stop, they won't resond until they are there at the corner.

     

    If however you told them to take ten steps and wait for further instructions....then they would respond a lot quicker.

     

    This is what your sketch is effectively doing

     

     

    However the buutons are troubling me...

    I understand that when you press a button, the pin goes high (+6v)  .... should be 5v

    If the button is a momentary button it should go to zero when released ...

    (You have not mentioned if you have external resistors that pull it down ...if not add a 220, 1K or 10K between pin2 and ground, and pin3 and ground.)

     

    In this case, your sketch would make it go one revolution only, not all the way to the other end.

     

    So I think we need to sort out your buttons first.

    Can you add a LED (WITH A SERIES RESISTOR!!) between Pin 4 and ground and Pin 5 and ground.

    and alter your sketch to add :-

     

    in void setup()


      int LedPin1 = 4;

      int LedPin2 = 5;

      pinMode(LedPin1, OUTPUT);

      pinMode(ledPin2, OUTPUT);

     

     

    then in void loop() ....

     

      if (buttonState1 == HIGH)

      {

      DigitalWrite(Ledpin1, HIGH);

      stepCount =2;               //This resets to a known state rather than continuing to count while the button is HIGH

      }

      else

      {

           DigitalWrite(Ledpin1, LOW);

      }

     

      if (stepCount >1)

      {               

          myStepper.step(stepsPerRevolution);     //stepsPerRevolution

      }

      if (buttonState2 == HIGH)

      {

         DigitalWrite(Ledpin2, HIGH);

         stepCount =-2;      //This resets to a known state rather than subtracting while the button is HIGH

      }

      else

      {

         DigitalWrite(Ledpin2, LOW);

      }

      if (stepCount  < 1)

      {          

         myStepper.step(-stepsPerRevolution);

      }

      Serial.println(stepCount);

    }

     

     

    Now the led should light when the button is pressed.

    I suspect your problems are due to the input pin 'floating', but the resistor and led should tell you this quickly.

    (You don't need to hook the stepper up for this test....)

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark,

        Yes, you are correct; the button input was floating. Finally solved the

    problem with a "while" sketch. Thanks for the LED test suggestion. It will

    prove helpful when assembling other parts of this very complex project.

        Another question: What is the best way to test the current of a

    salvaged power supply? The output voltage is 12 and 24v.

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Keith

    The floating inputs catch out people every now and then.

    I always prefer to use a pullup resistor (internal or external) and then switch to ground.

    It also means if you have a short, the 5v supply doesn't go.

     

    You could do some research on it, otherwise stick a load on it.

    12v automotive lamps are a good cheap source for 12v and 24v.

    Measure the voltage and see when it starts dropping off.

    You should be able to work it out by noting the current and the voltage.

     

    Chances are the capacitors will have aged, and you'll start getting large amounts of ripple.

    This may or may not affect your load.

     

    If your project is rather large and the loads are not constant, you could hang a battery across it.

    Use the supply to charge the battery/batteries, while the current for the load is sourced from the battery.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark,

        Thanks for the advise.  I am starting the final wiring. Will know the

    outcome in a few days.

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<