Arduino Forum Arduino GSM Shield QUECTEL M10 + Sparkfun RFID Eval with RFID Mod SM130 Mifare
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
  • Replies 0 replies
  • Subscribers 400 subscribers
  • Views 265 views
  • Users 0 members are here
  • rfid
  • gsm
  • arduino
Related

Arduino GSM Shield QUECTEL M10 + Sparkfun RFID Eval with RFID Mod SM130 Mifare

Former Member
Former Member over 12 years ago

Hello all.

 

I am doing a project where I have to send an SMS to a given phone number after someone swipes an RFID card on the reader.

 

Here is the hardware I am using (with Arduino IDE  1.0.5):

Arduino Uno R3 -> http://arduino.cc/en/Main/ArduinoBoardUno

Arduino GSM SHIELD -> http://arduino.cc/en/Main/ArduinoGSMShield

Sparkfun RFID Eval 13.56 Mhz -> https://www.sparkfun.com/products/10406

RFID Module - SM130 Mifare (13.56 MHz) -> https://www.sparkfun.com/products/10126

 

The problem here is that the GSM library (included in the IDE) conflicts with the SoftwareSerial library (used for the RFID). I have read a lot about these and i can't make them work together.

So my approach is now to make them both with the SoftwareSerial lib. With this i could assign the GSM shield to work with pins 2,3 and RFID with 7,8. Hopefully this will do the trick.

My next step is to send the SMS with AT COMMANDS, but I just can't seem to make this work. Has anyone used AT COMMANDS with the latest arduino GSM Shield? Can anyone provide me a working example code of this? I have been searching everything and still no luck.

 

Now on the bigger picture, has anyone done anything similar? How did you make it work? Am I using the right approach?

 

Much help is needed. Sorry for my English, I am Portuguese.

 

Thank you in advance.