Arduino
  • Products
  • More
Arduino
Arduino Forum Measure square wave frequency
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 421 subscribers
  • Views 5601 views
  • Users 0 members are here
  • square
  • arduino
  • frequency
Related

Measure square wave frequency

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I'm working with the Arduino Due ans I used the following code:

 

// period of pulse accumulation and serial output, milliseconds

#define MainPeriod 100

long previousMillis = 0; // will store last time of the cycle end

volatile unsigned long duration=0; // accumulates pulse width

volatile unsigned int pulsecount=0;

volatile unsigned long previousMicros=0;

 

void setup()

{

  Serial.begin(19200);

  attachInterrupt(6, myinthandler, RISING);

}

 

void loop()

{

  unsigned long currentMillis = millis();

  if (currentMillis - previousMillis >= MainPeriod)

  {

    previousMillis = currentMillis;  

    // need to bufferize to avoid glitches

    unsigned long _duration = duration;

    unsigned long _pulsecount = pulsecount;

    duration = 0; // clear counters

    pulsecount = 0;

    float Freq = 1e6 / float(_duration);

    Freq *= _pulsecount; // calculate F

    // output time and frequency data to RS232

    Serial.print(currentMillis);

    Serial.print(" "); // separator!

    Serial.print(Freq);

    Serial.print(" ");

    Serial.print(_pulsecount);

    Serial.print(" ");

    Serial.println(_duration);

  }

}

 

void myinthandler() // interrupt handler

{

  unsigned long currentMicros = micros();

  duration += currentMicros - previousMicros;

  previousMicros = currentMicros;

  pulsecount++;

}

 

to measure the frequency.

 

I can measure frequencies higher than 1.5kHz accurately, but I can't seem to measure lower frequencies.

 

How can I measure lower frequencies, say 400Hz and above?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    Hi Matt, I don't know about this situation but usually sampling over a longer time period will improve accuracy. John
  • D_Hersey
    D_Hersey over 12 years ago in reply to jw0752 +1
    John is right, there I said it! You might be able to get more accurate timing by latching the wdt upon interrupt. Reset the Arduino Due board using the watchdog - Arduino Forum
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey +1
    I tried setting mainPeriod to be longer but it still didn't measure accurately lower frequencies. Regarding the wdt , I don't understand how can it help, can you elaborate? thanks.
  • jw0752
    jw0752 over 12 years ago

    Hi Matt, I don't know about this situation but usually sampling over a longer time period will improve accuracy.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 12 years ago in reply to jw0752

    John is right, there I said it!

    You might be able to get more accurate timing by latching the wdt upon interrupt.

    Reset the Arduino Due board using the watchdog - Arduino Forum

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey

    I tried setting mainPeriod to be longer  but it still didn't measure accurately lower frequencies.

     

    Regarding the wdt, I don't understand how can it help, can you elaborate?

     

    thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 12 years ago

    Here are some DSs for early timer chips.  This functionality is typically integrated today, but is should give some basic insight as to what is going on in uP timing.  The more sophisticated your OS, the more difficult timing with your CPU becomes:

     

    http://liris.cnrs.fr/~mmrissa/lib/exe/fetch.php?media=mc6840.pdf

    http://www.z80.info/zip/z80ctc.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    try checking this out, sparkfun has a whole project but it is open source so yo can use and implement in your own way.

     

    key thing to look at is the sketch as it will have a working solution even if you display it in a different way

     

     

    https://www.sparkfun.com/products/10140

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 12 years ago

    Here is a great cookbook article on the topic of square waves.  No direct answer to your question here, but everyone who enjoys this site could probably learn something from it, just came across it today.  From our great friends at EDN:

     

    http://www.edn.com/design/test-and-measurement/4432218/Boost-and-modify-square-waves

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago

    This is the type of circuit where it may be good to maybe offload the core of it to external logic. Basically an external counter to measure the period, and the Arduino can read the counter once it is latched. There used to be tons of 10MHz and 50MHz frequency counter circuits doing exactly this, in 74xx logic gates and no Arduino, and displaying the output on LED displays. If you can't find anything and wish to pursue this method, let me know - I'm sure I can dig up such a circuit either on the Internet or in a book.

    EDIT: Although, just noticed, you're only interested in low single-figure kHz range? If so, Arduino should be sufficient.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ravi_butani
    ravi_butani over 12 years ago

    // mills() reference http://arduino.cc/en/Reference/millis
    // attachinterrupt() reference http://arduino.cc/en/Reference/attachInterrupt
    // Due pin 0,1,2 corresponding to pin interrupt 0,1,2 respectively
    // All the best from RAVI BUTANI
    // this code measures frequency only accurate for >100Hz
    // for less frequency minor modifications needed
    
    
    unsigned long time_stamp;
    unsigned int count0 = 0;
    unsigned int count1 = 0;
    unsigned int count2 = 0;
    
    
    unsigned int output0 = 0;
    unsigned int output1 = 0;
    unsigned int output2 = 0;
    
    
    void setup()
    {
      Serial.begin(9600);
      time_stamp = millis();
      attachInterrupt(0, sensor0, RISING); // sensor 1 on mega pin no 2 Due pin 0
      attachInterrupt(1, sensor1, RISING); // sensor 2 on mega pin no 3 Due Pin 1
      attachInterrupt(2, sensor2, RISING); // sensor 3 on mega pin no 21 Due Pin 2
    }
    
    
    void loop()
    {
      if(millis() - time_stamp > 50)
      {
        detachInterrupt(0); // disable interrups
        detachInterrupt(1);
        detachInterrupt(2);
        output0 = count0 * 20;
        output1 = count1 * 20;
        output2 = count2 * 20;
        Serial.print("Sensor0 Reading = ");
        Serial.println(output0);
        Serial.print("Sensor1 Reading = ");
        Serial.println(output1);
        Serial.print("Sensor2 Reading = ");
        Serial.println(output2);
        delay(40);
        count0 = 0;
        count1 = 0;
        count2 = 0;
        time_stamp = millis();
        attachInterrupt(0, sensor0, RISING); // we have done with this mesasurenment,enable interrups for next cycle
        attachInterrupt(1, sensor1, RISING);
        attachInterrupt(2, sensor2, RISING);
      }
    }
    
    
    void sensor0()
    {
      count0++;
    }
    
    
    void sensor1()
    {
      count1++;
    }
    
    
    void sensor2()
    {
      count2++;
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to ravi_butani

    Thanks for your reply.

     

    I tried that, it measures 1500Hz and higher quite accurately but anything below it and it fails.

     

    Do you know what else can be done to fix this?

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    did you checkout the spark fun link I provided, what was the result

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>