Arduino
  • Products
  • More
Arduino
Arduino Forum New Arduino IDE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 421 subscribers
  • Views 5153 views
  • Users 0 members are here
  • libraries
  • arduino
Related

New Arduino IDE

Workshopshed
Workshopshed over 11 years ago

There's been a few couple of upgrades to the Arudino IDE over the last month.

 

Arduino - Software

https://github.com/arduino/Arduino/blob/master/build/shared/revisions.txt

 

As I'm getting started with the Yun it's nice to see that some of the issues around that have been resolved but I think the feature I'm most interested in is the Library Manager, this should make working on different projects a whole lot easier.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago +4
    8 Minutes to download.... https://youtu.be/N1ug9-rhSs4?t=1m50s
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to neilk +3
    Neil, that's correct. Not only but I have explored a bit and see that the library manager is based on a JSON file including all the last updated library list organised by category. The json file is library_index…
  • WestfW
    WestfW over 11 years ago in reply to neilk +3
    > Microsoft standard software installation rules Sigh. I really hate the way that "Microsoft standard rules" scatter an application all over the disk :-(
  • WestfW
    WestfW over 11 years ago in reply to neilk

    I hear that 1.6.2 installs some of the compiler tools "on demand" rather than all at once.  No ARM compiler unless you install ARM boards with the new "board manager", for example.

    (and: this apparently causes some problems, especially with 3rd party hardware, since compilers are now in a different place on disk, and might not be there at all.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to WestfW

    WestfW I've also realised that in Windows, it now conforms more to Microsoft standard software installation rules, suggesting installation in ..../Program Files (x86) and also placing a large amount of stuff in .../AppData/Roaming/Arduino15

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to neilk

    Neil, that's correct. Not only but I have explored a bit and see that the library manager is based on a JSON file including all the last updated library list organised by category.

     

    The json file is library_index.json and is under the .../Arduino15 folder that is under Windows where you mention, Linux under the Arduino15 ide installation folder and in Mac OSX under /Users/_user_name_/Library/Arduino15 (this last can't be found with finder and should be reached by terminal.

     

    Every library is a json object, very simple to understand in the format like the following:

     

        {

          "name": "TinyWireM",

          "version": "1.0.0",

          "author": "Adafruit",

          "maintainer": "Adafruit \u003cinfo@adafruit.com\u003e",

          "sentence": "I2C library for Trinket and Gemma, adapted from BroHogan's code on Arduino Playground",

          "paragraph": "I2C library for Trinket and Gemma, adapted from BroHogan's code on Arduino Playground",

          "website": "https://github.com/adafruit/TinyWireM",

          "category": "Signal Input/Output",

          "architectures": [

            "*"

          ],

          "types": [

            "Recommended"

          ],

          "url": "http://arduino.cc/download.php?f=/libraries/TinyWireM-1.0.0.zip",

          "archiveFileName": "TinyWireM-1.0.0.zip",

          "size": 15696,

          "checksum": "SHA-256:6b5ee59e855d8415f9e5062e897c590acbbfeb8e93dbf118d47636c869915386"

        }

    Maybe a good idea that the community maintain a version of this file updated with the libraries that are not distributed by the Arduino's friends (e.g. Adafruit & company) but maybe very useful for the developers.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • WestfW
    WestfW over 11 years ago in reply to neilk

    >  Microsoft standard software installation rules

     

    Sigh.  I really hate the way that "Microsoft standard rules" scatter an application all over the disk :-(

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to WestfW

    I really hate the way that "Microsoft standard rules" scatter an application all over the disk :-(

    You and me both !! I borrowed the expression from a posting about 1.6.2 in another forum............not my own words image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    So far I've not found the new library manager to be of much help. I tried adding a library from zip and although that did create a library (in my user area) it did allow that library to reference other libraries which were in the program files folders. The net result was that it did not compile. I move the library over to the same folder structure as the others and it worked fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to Workshopshed

    But you can change somewhere in the settings (maybe in the preferences advanced text file) where the libraries are stored. Not sure if this version search in both places (your custom folder and the standard folder of the application) or if you should move all the libraries somewhere else.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to balearicdynamics

    Eagle CAD uses symbolic links which works quite well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to Workshopshed

    Also under Windows ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 11 years ago in reply to Workshopshed

    Workshopshed Hi Andy, my experience of installing libraries under Windows 7 is a bit happier:  under the 1.6.1 IDE,  I used the existing facility to install various libraries from their .zip files - they were installed in a folder called libraries, under the My Sketches Folder (which I keep elsewhere, and tell the IDE where to find it!!), not within the default Libraries folder.

     

    I subsequently used the provided uninstall program to remove 1.6.1 before installing 1.6.2. The libraries are still there; 1.6.2 can see them; I can load an example from one of them and it compiles happily.........I'm impressed.

     

    Separation of the downloaded IDE from "your own" stuff - sketches, external libraries etc seems to mark a big improvement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>