Arduino Forum RA8875 & tft 40 pin 7'' LCD
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
  • Replies 3 replies
  • Subscribers 402 subscribers
  • Views 563 views
  • Users 0 members are here
Related

RA8875 & tft 40 pin 7'' LCD

Former Member
Former Member over 10 years ago

Hello Im trying to display an image with an RA8875 controller and a 7 inch tft but i have noway of going about, doing so. Is there anyway that i can make something like this to work ? Any good recommendations will be take in consideration. But since i already have the products i would like to do it with just these items and the Arduino. I tried getting it running with the arduino uno but im having a lot of issues. The only thing i was able to do is get the screen to turn on. I followed the instruction and codes provided yet nothing happens on the screen. The only code that worked properly was the touch sensor code which displayed the coordinates of where im touching which is a good sign

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to Former Member +1
    Good to hear the bells of success. Just a small plug, could you mark my answer if it help solve this. thanks, clem
  • clem57
    clem57 over 10 years ago

    Did you follow these instructions for inst all of library? https://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use/arduino-libraries. If it has installed, did you try these examples https://github.com/adafruit/Adafruit_RA8875/tree/master/examples?

    The other thing to do is get a multimeter and check signals be correct.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago

    hey i successfully got it working pretty well thank you so much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Former Member

    Good to hear the bells of success. Just a small plug, could you mark my answer if it help solve this.

    thanks,

    clem