Arduino Forum Need some urgent help related to this Arduino Audio processing
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 828 views
  • Users 0 members are here
Related

Need some urgent help related to this Arduino Audio processing

Former Member
Former Member over 9 years ago

I am following this link from instructable site..

 

 

http://www.instructables.com/id/Arduino-Audio-Input/

 

My question is,

 

Instead of using the Microphone Radioshack 33-3038, which is listed in the tutorial , can I  use  https://www.sparkfun.com/products/9964,

 

KIndly suggest is there any modifications required in other parts for the circuitary If I go for Electret Microphone .

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2 suggested
    Hi Raviraz, Yes there is a difference between the two microphones. The 33-3038 is a dynamic microphone which means that it is a coil of wire in a magnetic field. Sound waves vibrate the diaphragm and this…
  • Former Member
    Former Member over 9 years ago in reply to jw0752 +1
    Thanks once again John. I am pretty new bee in Arduino. My basic theme is to calculate the frequency of the sound generating from my test device",So i have chosen this instructble to help. I will try to…
  • Former Member
    0 Former Member over 9 years ago in reply to jw0752

    Hi John,

     

      I have builded the circuit with LM741 opamp, and Can see values in serial as -1Hz always, not sure why it is happening, any help pls.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to Former Member

    If you have some way to check the input to the Arduino with a meter do so. We need to verify that the amplifier is working. If you have a signal generator you could also put an artificial signal into the Arduino to see if it is processing the input properly. Lacking this you can post your schematic and code so it can be looked at on the forum. If we are going to get help from some of the arduino coding experts they will need a clear explanation of what the code is suppose to do.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<