Arduino Forum HOW TO DRIVE A PIEZODEVICE
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
  • State Not Answered
  • Replies 14 replies
  • Subscribers 394 subscribers
  • Views 877 views
  • Users 0 members are here
Related

HOW TO DRIVE A PIEZODEVICE

Former Member
Former Member over 9 years ago

I used to be knowledgable in these things but I have had some health problems (stroke and heart attack)  which have left me with some  blank spots in my memory.

 

So I would appreciate some help on some things.

 

I want to drive a piezo device at about 50 or 60 Hz.  This will create a ping or beep.

I want it to pulse for a predetermined time each time I press a button.

Do I need current limiting resistors or driver transistor?

 

Is there any one who can help me with this?

 

bob

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2
    Hi Bob, Depending on how loud you need the sound to be you could conceivably drive the piezo directly off a 555 timer. There are also little piezo buzzers with a built in oscillator that could be incorporated…
  • michaelkellett
    michaelkellett over 9 years ago in reply to jonivanart +1
    Sorry Jon, I was replying to Bob when he said: I have seen on the internet if you put a piezo device in a small plastic container filled with mineral oil it will work as a transducer able to send out a…
  • clem57
    clem57 over 9 years ago +1
    Why not use sonar? C
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to clem57

    I thought that was what he was asking about:

     

    from Wiki:

     

    Sonar (originally an acronym for SOund Navigation And Ranging) is a technique that uses sound propagation (usually underwater, as in submarine navigation) to navigate, communicate with or detect objects on or under the surface of the water, such as other vessels.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    That is exactly trying to make a low priced homemade sonar unit of sorts

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago

    Ok let me try to straighten some things out here.

    First it should be vegetable oil and not mineral oil.

    by putting the piezo device in the oil and in a plastic bottle it is  water proofed.  When you put a say 60 Hz tone on the piezo the sound waves travel through the oil into the water and you have low cost trans ducer to send out a signal for your home made low cost SONAR unit.

     

    That is the thoughts anyway. now to test the thoughts out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    The pattern of the sonar “wave” won’t necessarily be so different in water from that in air per sé, but the speed of the wavefront will be much faster in the much denser water. The main problem I imagine you would have using a transducer underwater that was designed for service in air, and vice-versa, is the frequency of operation. Most “sonar” transducers designed for use in air are ultrasonic, and the signal they produce will lose most of its useful energy within a very short distance underwater. Underwater sonar operates at a much lower frequency, and will not be effective at distance in an air medium.

    http://societyofrobots.com/robotforum/index.php?topic=158.0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<