Arduino Forum AUTOMATED BLIND
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
  • State Suggested Answer
  • Replies 13 replies
  • Answers 6 answers
  • Subscribers 395 subscribers
  • Views 1171 views
  • Users 0 members are here
Related

AUTOMATED BLIND

Former Member
Former Member over 9 years ago

Am having a project to deliver in two months time, the project is about automated window blinds. Am good in computer programming but not actually good in electronics. I need assistance please.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago in reply to Former Member +1 suggested
    Hi Benny For everything electro-mechanical that is created there isn't one path to success. Your imagination and your available technology will determine how you get the job done. That is why it is difficult…
  • kulky64
    kulky64 over 9 years ago in reply to Former Member +1 suggested
    Please, if there is another component that is needed for the system you can let me know. Maybe some limit switches or some other way to detect if the blinds are in their extreme positions. Another question…
  • Former Member
    Former Member over 9 years ago in reply to jw0752 +1
    Have gone through Ben Heck Video, but the concept he used doesn't really suit what am meant to work on. It's the same ideology with mine but, his concept his based on bluetooth but i want mine to be autonomous…
  • jw0752
    0 jw0752 over 9 years ago

    Hi Benny,

     

    Here is a post from 2014 that may have some ideas for you. You may be able to find other posts about Shades, Curtains, and window treatments by searching the E-14 Forum. Otherwise you will have to frame up your idea better and present it with specific questions so we have something to work with. As it is now it is too general.I look forward to following your progress.

     

    https://www.element14.com/community/community/experts/benheck/blog/2014/03/28/arduino-powered-curtain-automation

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to jw0752

    Thanks for the Hints.

    Have made some research, and the major component that i think i might require are LM35, LDR, a DC Motor and an Arduino UNO R3 board.

    I also which to make use of a Roman blind for a Demo. I don't know how appropriate the use of those components are?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to Former Member

    Hi Benny

     

    For everything electro-mechanical that is created there isn't one path to success. Your imagination and your available technology will determine how you get the job done. That is why it is difficult to tell you what components you will need. Try to break the system down into pieces and make the individual parts work and then interface them. I am not sure what an LM35 is and perhaps the LDR is a low dropout regulator. You will need a power source for the motor that is separate from the Arduino's power suuply. If you do want to power both the Arduino and the Motor off the same supply you will need a regulator and filter capacitors to make sure the Arduino get proper and clean power. The arduino will not be able to switch the motor on and off by itself. It will need a transistor that it can control that in turn will turn the motor on and off. The transistor will need to be protected with a flyback diode. If you are going to want the motor to rotate in both directions you will need a circuit called an H Bridge. An H-Bridge will allow the arduino to turn the motor in a CW or CCW direction as well as brake or stop the motion.

    The break down of your project might be:

     

    Arduino and software to interpret your input switch or switches. You could have one button to open the blinds and a second to close them. Or you could have one button that alternately opens and closes. Your software will have to accommodate switch bounce. The is where switches do not make a perfect closed contact immediately and the Arduino is fast enough to misinterpret this as multiple pushes of the switch.

     

    H-Bridge and Motor circuits. Here you will want to make sure that the H-Bridge powers the motor and that simulated input to the H-Bridge does what you expect it to do. This will also give you information on what will be required from the Arduino as Outputs to make the H-Bridge work.

     

    Motor to Blinds mechanical. Here you will have to devise a way for the motor to provide the power and motion necessary to open and close the blinds. It may be necessary to gear the motor down so that there is enough force to move the mechanism and also to slow it down so that it doesn't happen too fast.

     

    If you begin to work on this you will learn a lot and have a lot of fun. If you have questions someone on the Forum will try to help but we work best when you already have a partially working circuit and can give us drawings, pictures and schematics of what you have done.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bodhi_94
    0 bodhi_94 over 9 years ago

    The article on ben hack show is very helpful to you element14's The Ben Heck Show .. Get the idea from it.. And build your idea on it.. I think that is the best thing you can do..image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kulky64
    0 kulky64 over 9 years ago in reply to jw0752

    I am not sure what an LM35 is and perhaps the LDR is a low dropout regulator.

    The LM35 is temperarue sensor with analog output and by LDR he probably means Light Dependent Resistor to automatically adjust the blinds according to light conditions in the room.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to kulky64

    Hi kulky64,

     

    Of course you are right. I have worked with the LM35, 36, 37 series in the past but for some reason when I saw the number it didn't ring a bell. Also when I tried to search the number on Octopart it didn't come up. As far as the LDR is concerned you are probably right on that one too. Since I began on E-14 one of my pet peeves has been the use of unidentified acronyms and initialisms in posts. I began to collect them and identify them. To date I have a list numbering a little over 500 different XYZ, PDK, TTP, type codes that have been used. Here is a link to the post in case you are interested in looking at it. I just brought it up to date.

     

    https://www.element14.com/community/people/jw0752/blog/2014/10/03/acronyms-initialisms-abbreviations-and-variables

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago

    Yea, thanks for the brief explanation @John & kumarage.

    Am beginning to get more clue to the project. As you guys have rightly said, the LM35 is the Temperature/Heat Sensor that will bring in analog data that will be utilized by the motor. Also the LDR is the light Dependent Resistor that will also control the motor based on the brightness and darkness of its surrounding. To move the motor in both CW & CCW direction, a H-bridge (L239D) will be needed. Two switches will also be used to control the mechanism in both Automatic and manual mode. For sure a seperate power source will be required by the motor different from that which will power the arduino board. There will also be a fixed Gearing set which will initiate the relationship between the blinds itself and the electro-mechanical component to form a system. These are the components i can figure out for now  and i think  may be best suitable for the project.

    There is this IDE i downloaded for running my sketch, it's called FRITZING IDE, actually am still trying to get acquainted to it. Am using  Arduino IDE too.

    Please, if there is another component that is needed for the system you can let me know.

    Another question is since am going to be using an H-bridge, is there any need to use a transistor and a diode that will  be needed to  protect the circuit for flyback  charges from the motor.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kulky64
    0 kulky64 over 9 years ago in reply to Former Member

    Please, if there is another component that is needed for the system you can let me know.

    Maybe some limit switches or some other way to detect if the blinds are in their extreme positions.

    Another question is since am going to be using an H-bridge, is there any need to use a transistor and a diode that will  be needed to  protect the circuit for flyback  charges from the motor.

    Depens whether you will be using L293 or L293D. From page 7 of the L293 data sheet (www.ti.com/lit/ds/symlink/l293.pdf):

    "On the L293, external high-speed output clamp diodes should be used for inductive transient suppression. On the L293D, these diodes are integrated to reduce system complexity and overall system size."

    If your motor draws less than 1A (or less than 600 mA for L293D), then you don't need any transistors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to kulky64

    Tanks for that intro.

    Maybe some limit switches or some other way to detect if the blinds are in their extreme positions.

    I also thought about that but the only possible solution i was able to get is to utilize the ability to control the speed and OFF &ON time of the DC motor to control the extent to which the blinds can go. If am to use a limit switch please how will i incorporate that into the system, interms of coding and electronically?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    And for the H-bridge (L293 and L293D), i have gotten the whole gist.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>