Arduino Forum How to detect usage of height adjustable table?
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 394 subscribers
  • Views 1475 views
  • Users 0 members are here
  • barometric sensor
  • motion detecting
  • accelerometer
  • proximity sensors
Related

How to detect usage of height adjustable table?

svendsen2032
svendsen2032 over 8 years ago

Hi at element14

 

 

We have been trying to solve this matter for quite some time now, and we simply haven't been able to come up with a satisfying solution. We are working on a little "bot" placed on top of a height adjustable desk. The bot has to measure whether the desk is in a sitting or standing position. So we do either need to measure the movement and direction of movement or the height of the table. We have had some luck using proximity sensors (IR and US), but they are very dependent on the environment and placement, as e.g. a desk lamp can make the readings worthless.

 

 

We are now working with an accelerometer and/or a barometric sensor, but the acceleration of a table is very small and the height difference of the table is only 20-40 cm's. So the sensors have to be very precise and sensitive.

 

 

Soo, do you maybe have other ideas to what sensors we could use? Or maybe some insights into how we can get the accelerometer and barometric sensors to work properly? - would be a of great help image

 

Best regards Mads

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to svendsen2032 +2 suggested
    So we are trying to register everytime the users changes working position from sitting to standing and from standing to sitting You could use an ultrasonic sensor and detect the height to the ceiling.…
  • DAB
    DAB over 8 years ago +1 suggested
    Hi Mads, Have you considered using a capacitive sensor mounted to the desk? The TI sensor system can accurately detect objects up to about 50 cms. Another way would be to use a light and a camera to measure…
  • vandia
    vandia over 8 years ago +1 suggested
    On the note of what you're trying to do, you've giving detail of your method, but it still leaves your end goal rather vague.... especially with "acceleration of a table". It leaves the questions: "Is…
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to mcb1

    Mark, I think this solution is totally reliable with a very low impact. It has been successfully used by the first drones to detect their height and avoid terrain obstacles. There instead a sensor needed together. Suppose you stay sit on the the desk and it is not rare that your feet impact the sensor. Ok, it can be placed in a very good position but the risk always exists; When I sit to a desk I can have to put downside my backpack, my skateboard, my shoes to wear a more comfortable pair while I am working and so on (these are all real situations I saw while working in the Netherlands past year). So to avoid the ultrasonic (the best solution anyway) is wrong a second sensor should be added to confirm that it is the table moving and not the ground or some part of it.

    Also for this I see more than one easy solution:

     

    • If electronic movement it is sufficient to detect when the motor is on (no matter where it moves, the sensor detect the distance from the gorund (or the relative distance if something is on the ground in that moment).
    • If manual movement a cap sense placed in proximity of the desk unlock lever is another possible solution for bare mechanical movement
    • An inertial accelerometer is sufficient put beside the table to inow that it is the table moving instead the rest.

     

    Not only but the ultrasonic sensor is able with fewl ines of code to self-calibrate to a relative height when something is put under the table.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rsc
    0 rsc over 8 years ago

    Show us a picture of the table, and we can tell you good places to put sensors.

    Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<