Arduino Forum Voltage Max on ATMEGA328 Analog Inputs?
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
  • State Verified Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 399 subscribers
  • Views 4563 views
  • Users 0 members are here
  • analog inputs arduino
Related

Voltage Max on ATMEGA328 Analog Inputs?

jw0752
jw0752 over 8 years ago

Does anyone know what the max voltage that can be applied to the analog inputs of the ATMEGA328 Arduino uP? I know that it will convert 0V to 5V but how much tolerance does it have for voltages over 5 volts?

 

Thanks

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +7 verified
    From the Atmega328 manual Mark
  • Problemchild
    Problemchild over 8 years ago in reply to mcb1 +3 suggested
    Amazed at the high voltage capability on the Reset...obviously expecting abuse there! One thing to note is that your signal doesn't have any transients otherwise you'll need to take those in to account…
  • shabaz
    shabaz over 8 years ago in reply to Problemchild +3 suggested
    Hi John! That may be some old-school Flash mem programming voltage pin for non-in-circuit programming. Not sure, I didn't check the datasheet, but I recall a load of Flash devices requiring 12V.