Arduino
  • Products
  • More
Arduino
Arduino Forum Ethernet problem sending null characters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 418 subscribers
  • Views 2921 views
  • Users 0 members are here
  • client
  • client.print
  • ethernet
  • client.write
Related

Ethernet problem sending null characters

e14 Contributor
e14 Contributor over 13 years ago

Thank you in advance for your kind help.

I am using the Ethernet Library (client.print function) to access an electronic device which supports TCP/IP.

I must send a command string to the device that contains several NULL characters. I cannot send the string since the first NULL character terminates the transmission.

I tried sending 1 byte at a time and that works when sent to a VB.NET simulator that I wrote, however, it doesn't work with the device I am trying to use. I think the device may be expecting the entire command to be contained in a single packet. I tried using a string object and that didn't work either.

I need to be able to specify the data and its length and send it as a single packet.

Can anyone out there help me ?

Thanks,

Nick

Attachments:
EthernetCode.txt.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1 +1
    Mark, I haven't tried with firefox, but I doubt that would make a difference. Be sure to copy & paste the quoted material first into your draft post before highlighting it in the draft, and then clicking…
  • billabott
    billabott over 13 years ago +1
    make a quote out of something you paste into a message, you don't have to quote the previous message, then delete everything in the quote, and then paste into the empty quote. In Firefox, the e14 UI Editor…
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor +1
    Be sure to copy & paste the quoted material first into your draft post before highlighting it in the draft, and then clicking the "quote" icon. Are that be the difference ..... I wasn't pasting it in and…
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    As I understand it:

    1:  the serial device is attached to SOME piece of hardware

    2:  the hardware on the receiving end does a conversion from TCP/ethernet to serial data input to the device

    3: you are convinced that the embedded NUL character is a problem

     

    I suggest that you then MUST encode the data to successfully transmit packet.

    Opt A:  Invert all the bits

    Opt B:  Interleave binary 1s  via XOR 0x11 with every byte.

    Opt C:  Add binary 1 to every byte.

     

    It follows that you will have to implement a decode capability on the receiving side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<