Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sensor to detect Human Presence
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 81 replies
  • Answers 34 answers
  • Subscribers 442 subscribers
  • Views 16778 views
  • Users 0 members are here
  • human
  • detection
  • internet_of_things
  • arduino
  • sensor
Related

Sensor to detect Human Presence

gunaseelan
gunaseelan over 12 years ago

Hello Friends,

 

                    Is there any sensor to detect human presence . Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence . Another way is by using image processing technique. Kindly suggest me a better solution image .

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +7 suggested
    Hi Gunaseelan, OMRON do a thermal sensor that can detect stationary thermal objects as opposed to standard PIR motion sensor that only detect motion. The OMRON D6T thermal sensor is able to detect the…
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz +6 suggested
    shabaz Voight-Kampff machine ? Voight-Kampff machine | Off-world: The Blade Runner Wiki | FANDOM powered by Wikia
  • shabaz
    shabaz over 7 years ago in reply to dougw +5 suggested
    Agree.. I don't know why the OP excludes image processing - due to incorrectly perceived difficulty, or for a non-technical reason. I can understand the desire to possibly exclude due to (say) security…
  • robg713
    0 robg713 over 8 years ago

    Hi there Gunaseelan, was curious of what kind of things are happening that you would suspect the  presence of a human or humans? If you dont mind letting me know because i have a situation similar to you an cant figure out how to prove it and/or end it an its aggravating the *** out of me. So was curious if anything worked for you in your situation an if so please tell because i have to put a end to this. Thank you in advance for your time!!!!                            An if theres anyone here that has any info please do tell an thank you also in advance!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to robg713

    A motion detection spy video camera costs about $5. They work surprisingly well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alfredmuzinde
    0 alfredmuzinde over 8 years ago in reply to dougw

    l want to mange student who visit the dinning hall by detecting faces because the old method which we used promoted repeated meals and intruders  . student should enter the dining once per meal like breakfast or lunch . howbest can l tuckle such a scenario and what scencors can l use

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to alfredmuzinde

    I think the best method is a deterrent, because catching someone in the act and trying to intercede requires an enforcer to be present.

    If you use a biometric access control system such as facial recognition or fingerprints it may not work very well or it can get expensive and it is tedious to enroll everyone properly.

    If you use a simple video recorder which can be analyzed at a later time it may identify chronic offenders or it may deter abuse.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 8 years ago

    PIR sensor they are cheep and gets the job done !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to gsgill112

    Hi Gurinder, the OP specifically rules out PIR sensors:

    Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence .

    Anyway, I don't think a sensor exists to 'detect' humans, just some limited characteristics that humans have (and often these characteristics are not exclusive to humans either). Image recognition usually identifies anything that looks human-shaped. PIR detects anything warm that moves (cat or dog would be included). Also, plenty of 'human interaction' robots are designed to look and move like humans. They can speak too. Short of some intrusive surgery or extracting DNA, or interrogating and hoping that intelligent responses are present for only humans (and how long before this fails too?) I can't see how a machine or a sensor could 'detect' humans. Most of these characteristics can be faked too.

    This might sound pedantic but it's not any more, especially when cameras etc are used to unlock phones and PCs these days.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 8 years ago in reply to shabaz

    Correctly pointed out shabaz image I might have forgotten that while going through the comments, I agree , its difficult to figure out human presence if you are not using any kind of Thermal / Image sensing !

    Jee, sorry for the stupid comment image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to gsgill112

    Hi Gurinder,

     

    No worries, to be honest most of the comment was really for the OP anyway, since the question can't have a real answer without some significant bounds/limitations.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 8 years ago in reply to shabaz

    It's interesting to read through the comments as no one is focusing on the use of multiple sensor configurations to detect human presence. A single PIR certainly can't determine human movement from some other heat source movement but using multiple PIR sensors could.

     

    Imaging technology via a single lens configuration, for example, still only provides a 2 dimensional picture which does not always return the correct answer, so in my opinion, the ideal, more accurate, scenario would be to try and create a 3-d representation using multiple sensor types. Additional "dimensions" could include things like body mass, for example, which is a proven criteria to differentiate objects.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to BigG

    Hi! Indeed, times have changed, and a device can use processing and multiple sensors to get closer to extracting the desired knowledge of human presence.

    I forget the name, but there are commercial products that are used for unlocking doors, that use 3D information to detect facial features. I've seen one in action, you just have to stare into it for a couple of seconds.

    It shows the face on the screen but only for centering purposes, and instead it is measuring the distance to different features on the face. But I don't know if it can be fooled with something that is three-dimensionally like a human : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<>