Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino LCD Timer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 419 subscribers
  • Views 1887 views
  • Users 0 members are here
Related

Arduino LCD Timer

e14 Contributor
e14 Contributor over 12 years ago

Hi All,

 

I am making a model rocket launch controller, it features a safety, Arm switch, a launch button, and a 16x2 LCD display. So to launch the rocket you Arm the Rocket by flipping the arming switch. Then you turn the saftey key, which is an electronic safety. A HIGH signal is passed through the key switch, which allows the rocket to launch. here is my current code.

 

#include <LiquidCrystal.h>
LiquidCrystal lcd(2,3,4,5,6,7);


//Define Booleans
boolean Armed = true;
boolean Safe = true;
boolean DeArmedTestPassed = false;
boolean HasLaunched = false;
boolean Launch = false;
//Define Pins
int ArmPin = 8;
int SafePin = 9;
int LaunchPin = 10;
int Piezo = 11;
int Igniter = 12;
int SwitchLed = 13;
int PotPin = 0;


char * erase = "                ";


int PotVal = 0;


void setup()
{
pinMode(ArmPin, INPUT);
pinMode(SafePin, INPUT);
pinMode(PotPin, INPUT);
pinMode(LaunchPin,INPUT);
Serial.begin(9600);
lcd.begin(16,2);




    for(int i = 0; i <= 2; i++)
      {
lcd.setCursor(0,0);
lcd.println("    Welcome To    ");
lcd.setCursor(0,1);
lcd.println(" Rocket Launch 1 ");
delay(1000);
lcd.setCursor(0,1);
lcd.println(erase);
lcd.setCursor(0,0);
lcd.println(erase);
delay(1000);
      }


lcd.clear();



   for(int j = 1; j  < 3; j++) // CHANGE ME
     {
    lcd.setCursor(0,0);
    lcd.print("   Loading      "); //10
    delay(500);
    lcd.setCursor(10,0);
    lcd.print(".");
    delay(500);
    lcd.setCursor(11,0);
    lcd.print(".");
    delay(500);
    lcd.setCursor(12,0);
    lcd.print(".");
    delay(500);
     }
lcd.clear();

if(digitalRead(ArmPin) == HIGH)
  DeArmedTestPassed = false;

else if(digitalRead(ArmPin) == LOW)
DeArmedTestPassed = true;

digitalWrite(13,LOW);
}


void loop()
{

  if(DeArmedTestPassed)
      {
    PotVal = (analogRead(PotPin), 0, 1023, 0, 120); //Figure me out
    lcd.setCursor(0,0);
    delay(100);
    if(digitalRead(ArmPin) == HIGH && !HasLaunched)
        Armed = true;
    else
        Armed = false;
    if(digitalRead(SafePin) == HIGH)
        Safe = true;
    else
        Safe = false;
        if(digitalRead(LaunchPin) == HIGH)
        Launch = true;
   
    if(Armed)
      {
        lcd.setCursor(0,0);
        lcd.print("Status    Armed ");
        delay(250);
        HasLaunched = false;
      }
    else
      {
        lcd.setCursor(0,0);
        lcd.print("Status  Un-Armed");
        delay(250);
      }
    if(Safe)
      {
         lcd.setCursor(10,1);
         lcd.print(" SAFE ");
      }
    else
      {
         lcd.setCursor(10,1);
         lcd.print("      ");
      }


    if(Armed && !Safe && !HasLaunched)
    {
     lcd.setCursor(9,1);
     lcd.print("LAUNCH");
     delay(150);
     lcd.setCursor(9,1);
     lcd.print("      ");
     delay(150);
    }
   
    lcd.setCursor(0,1);
    lcd.print("T 00:00");
     }


    else if(!DeArmedTestPassed)
      {
         lcd.setCursor(0,0);
         lcd.print("Please de-arm   ");
         lcd.setCursor(0,1);
         lcd.print("device & reset");
      }
      if(Armed && !Safe && !HasLaunched &&  Launch)
      {
       lcd.setCursor(8,1);
       lcd.print("LAUNCH!");
       digitalWrite(13, HIGH);
       delay(1500);
       digitalWrite(13, LOW);
       lcd.setCursor(8,1);
       lcd.print("        ");
       Launch = false;
       Armed = false;
       HasLaunched = true;
      }
}

So here is my problem. I will have a 10k pot. And as I turn it I want the time displayed(mock up at line 140)  to increase to 2:00 when the pot is at max, and 00:05 at 0 pot. And once the system is unsafe and armed, you can initiate the launch. Once the launch is initiated it will count down and update the display to the new time every second. I have absolutely no idea how to set up the timer and display the decreasing time. I know I will have to use some form of a for loop. Bout it image

Thanks Guys,

 

Austin

  • Sign in to reply
  • Cancel

Top Replies

  • kidiccurus
    kidiccurus over 12 years ago +1
    Wow, another arduino detonator, there seem to be a lot of them at the moment. Not the answer to your question but lines 29 to 32, shouldn't at lest one pin be set as output.
  • kidiccurus
    kidiccurus over 12 years ago in reply to nschreiber0813 +1
    You rember I said there were a lot of detonators at the moment. This is what I was taking about (Noah). I also have a friend working on a simple microcontroller free version.
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Hey Noah, I will record a little video later showing you the progress I have made. If you want to talk about it email me at austin2118ace@gmail.com this is not the best place to discuss it. -Austin
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to kidiccurus

    Owe that is a shame. You should try convincing him otherwise because there seems to be a lot of people wanting to build something like this so I think it would be fairly popular.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hey Guys,

    So I have found some code I believe will work, but I need to repurpose it for my LCD, since the original code uses a 7 Segment display.

    int potPin = 0;
    int seconds = 0;
    int h = 0;
    
    
    
    
    //Format Display #:## for greater than 60 seconds
        if (seconds >= 60){
          segment.drawColon(true);
          segment.writeDigitNum(0, 0);
          segment.writeDigitNum(1, (seconds/60)); //minutes
          segment.writeDigitNum(3, (seconds % 60)/10); //tens of seconds
          segment.writeDigitNum(4, (((seconds % 60) % 10))); //seconds
          segment.writeDisplay();
        }
       
        //Format Display ##.# for less than 60 seconds but greater than 10 seconds
        if (seconds >= 10 && seconds < 60) {
          segment.drawColon(false);
          segment.writeDigitNum(0, (seconds/10));
          segment.writeDigitNum(1, (seconds % 10), true);
          segment.writeDigitNum(3,0);
          segment.writeDigitNum(4,0);
          segment.writeDisplay();
        }
        //Format Display #.## for less than 10 seconds
        if (seconds < 10) {
          segment.drawColon(false);
          segment.writeDigitNum(0, 0);
          segment.writeDigitNum(1, seconds, true);
          segment.writeDigitNum(3,0);
          segment.writeDigitNum(4,0);
          segment.writeDisplay();
        }
       
       
         //segment.println(seconds);
        //segment.writeDisplay(); 
       
        //Button
        button = digitalRead(inPin);   // read the input pin
        //Serial.println(button);
    
       delay(10);
      }
    
      if (button == 0 ){ //Code for Launch Button Pressed
        Serial.println("LAUNCH");
       
        //Play Sound
        tone(speakerPin, 700);
        delay(250);
        noTone(speakerPin);
        tone(speakerPin, 800);
        delay(250);
        noTone(speakerPin);
       
        h = seconds * 100;
       
       for (h!=0; h--;){
        
            if (h >= 6000){
              //Format Display ##:## for greater than 60sec
              segment.drawColon(true);
              segment.writeDigitNum(0, 0); //tens of minutes
              segment.writeDigitNum(1, (h/6000)); //minutes
              segment.writeDigitNum(3, ((h % 6000)/1000) % 10); //tens of seconds
              segment.writeDigitNum(4, (((h % 6000/100) % 10))); //seconds
              segment.writeDisplay();
              }
             
            //Format Display ##.## for less than 60 seconds 
            if (h < 6000) {
              segment.drawColon(false);
              segment.writeDigitNum(0,((h % 6000)/1000) % 10); //tens seconds
              segment.writeDigitNum(1, (((h % 6000/100) % 10)), true); // seconds
              segment.writeDigitNum(3,(h % 100) / 10); // tenths of seconds
              segment.writeDigitNum(4,(h % 100) % 10); // hundredths of seconds
              segment.writeDisplay();
             
           
            }
           
            //Play sound last 10 seconds
            if (h <= 1000) {
              if (h == 1000 ){
                tone(speakerPin, 800); //Play sound
              }
                if (h <= 1000 && (h % 100) / 10 == 0 && h > 50){
                tone(speakerPin, 800); //Play sound
              }
               if ((h % 100) / 10 == 8) {
                  noTone(speakerPin);}
             }
            
             //Play sound every 30 seconds (1:30, 1:00, 30.0)
           
            if (h/100 == 30 || h/100 == 60 || h/100 == 90 && (h % 100) / 10 == 8){
              tone(speakerPin, 800); //Play sound
            }
           
             if ((h % 100) / 10 == 8) {
                  noTone(speakerPin);
                }
                 
            delay(10);
        }

     

    So how would I change this code to work with a LCD, my time is wrote at 3,1 on my LCD as 00:00.

                                                                                      

    Thanks,

    Austin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    using an LCD display is far simpler than using the 7 segment displays

     

    Firs you get the correct library installed for you LCD display

     

    In your code you will create an instance of it similar to this "LCDLIB LCD = LCDLIB(20,2) // 20 characters by 2 lines

     

    then after a couple of other initialization statements you will just do something like this

     

    LCD.write(0,0,"Hello"); // hello on the first line, left side

    LCD.write(1,0,"Time left: "); // time remaining on the second line, left side

    LCD.write(1,11,Time); // wire the time variable / string to the second line position 12

     

    so as you can see, way simpler, when you get an LCD shield you will get sample code that will elaborate on all this but as you can see it is much simpler than the 7Segment displays

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    I can agree it is much simpler. I have the library, this is a snippet I got on GitHub, the full code is in the first post.

     

    I guess I really just need to know how to format it, So if Seconds is over 60, print 01:00 and when it isn't not to.  Along with updating it as it is counting down.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<