Arduino
  • Products
  • More
Arduino
Arduino Forum Experience with a humidity sensor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 1988 views
  • Users 0 members are here
  • sensors
  • humidity
Related

Experience with a humidity sensor?

e14 Contributor
e14 Contributor over 11 years ago

I'm working on an Arduino project logging humidity, temperature and air pressure in a sewer for 30 days at a time. The environment is very hostile, 99 - 100% humidity and full of sulphuric acid.  (The acid comes from hydrogen sulphide combining with the humidity).  The prototype works fine and I'm about to make the final version of the hardware for deployment into the sewer.

 

I'm using a HYT 221 humidity sensor and while it is supposed to be chemical resistant I have the funny feeling it is not going to last the desired month in the sewer.  I suspect that the housing I'm going to use (Jiffy box) will allow moisture in, even with an o-ring around the sensor.  I also need to have the air pressure sensor exposed and that has no filter or protection.

 

Has anyone else had any experience exposing sensors to hostile environments and not having them die?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    i remember we used coffee straws (q-tips may work too) or whatever to cover pin holes during the 'ruggedizing' process. Used to purchase consumer products and convert them to military grade products. good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    Here is a little datasheet about Si RTV:

     

    http://www.silicone.jp/e/catalog/pdf/rtv_ele_e.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    That is definitely so.  If you are going to go the RTV route, you have to mount your box solidly and use a good mechanical strain relief on any cables.  Cable clamps used with the proper hardware can help.  You can get stuff like this:  RF PARTS CW10B | BLACK 1 IN WIDE X 10 FT LONG COAX WRAP ROLL

     

    You should be able to get a cast aluminum project box that features an o-ring seal.  Those are pretty water-tight when used rightly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    These guys built a psychrometer:

     

    http://www.edn.com/design/sensors/4430083/Measure-RH-with-instrumentation-grade-system-monitor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<