Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum I am not a smart person, but I do like performing a bit of science
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 414 subscribers
  • Views 4759 views
  • Users 0 members are here
  • humidifier
  • water measurement
  • arduino
Related

I am not a smart person, but I do like performing a bit of science

cstanton
cstanton over 4 years ago

It's too warm in the United Kingdom, so I figured I'd invest in a fan/humidifier combo. 

image

The downside to this hardware, is that it will burn itself out. There's nothing detecting when the water reservoir doesn't have water in it. It's convenient enough, 3 modes to the fan, 3 levels of humidifier, battery, and USB rechargeable. 

So I figured, why not try to detect how much water is left in it with the hardware I have available? I couldn't wait for looking up too much detail or ordering parts from an online store.

I've no idea what I'm doing, so I figured, let's stick a couple of paperclips in there and connect it to an arduino uno.

image

So I read a bunch of values, do some buffering with an array, average them out. I get a very rough sine wave into the analog pin.

And then I notice the pattern, the water's low, the values are higher, the water's high, the values are lower. Setup some ranges, great.

Then I realise what I'm measuring when I turn off the humidifier, the paperclips are picking up the electrical noise from the humidifiers in the water

image


Not quite how I expected to measure if there's water left, but it appears if it's working harder, it's easier to pick up the noise, water isn't the best electrical conductor after all.

Still, I'm sure I should find a better method, but it is a small reservoir, I considered 3D printing something to be able to screw a bottle in to expand it a bit more though.

What do you think?

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 4 years ago +6
    I suppose it will take a mechanical engineer to solve this :-) Make a capacitor by twisting about 600mm of 26 AWG insulated wire together for use as the sensor. Or whatever small diameter wire is at…
  • beacon_dave
    beacon_dave over 4 years ago in reply to cstanton +2
    I wouldn't have expected a steam based humidifier to be USB/battery powered. Some of the evaporative ones just blow air through a wicking filter or use ultrasonics or an impeller to create a mist that…
  • skruglewicz
    skruglewicz over 4 years ago +1
    Hi cstanton .. As we say in Boston Massachusetts USA, your "Wicked Smart" and your "Wicked PISSA" too .... Seriously I would have never thought of that. I found an easier way to measure water level…
  • beacon_dave
    beacon_dave over 4 years ago in reply to Andrew J

    Perhaps use make use of the QTouch feature of the AVR ?

    Embedded World 2015: QTouch-Based Water Level Sensing
    https://www.youtube.com/watch?v=MY33xg83gnM

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to cstanton

    Humidifiers are awesome! : ) 

    The one I have works like Dave mentions, i.e. it only blows cold air through a material that wicks up water from the bottom, i.e. it's ok to run it dry. If your model doesn't have a wick material (the wick is usually replaceable to prevent using mouldy ones) then it could be using a different mechanism, but I'm not very knowledgeable on other methods.

    Parts are getting hard to find, but if you can find a humidity sensor, that would be a good addition just attached to the side of the unit, since the amount of humidity will be easily picked up by the sensor (hopefully!), just for observing your room status and the impact of the humidifier. 

    Regarding adding a bottle, that's a good idea (some mechanism may be needed to stop the water if the reservoir is full, the one I have uses mechanical means, like a float I think (not sure).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 4 years ago in reply to beacon_dave

    Tap water is quite conductive.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago
    cstanton said:
    I couldn't wait for looking up too much detail or ordering parts from an online store.

    Guys, I think this is the key line: what can be done with what is to hand rather than buying sensors or such.  Obviously, we don't know what Chris has to hand but I'm assuming for this experiment, little more than resistors, capacitors, wires, battery, Arduino and the like.  I guess it's ok to assume standard household stuff as well: perhaps a cork, paperclip(!), plastic milk bottle cap, wire coat hanger etc.  Simple stuff.  It's an interesting problem.  So suggestions that don't require logging on to a parts store!

    "....detect how much water is left" is a different proposition to "...is it about to get empty" as it implies either steady readings as the water level drops, or an indication of the water level at pre-specified points, e.g. 3/4, 1/2, 1/4, 1/8 full.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago

    I suppose it will take a mechanical engineer to solve this :-)

    Make a capacitor by twisting about 600mm of 26 AWG insulated wire together for use as the sensor.  Or whatever small diameter wire is at hand.  A hand drill works great for this.

    image 

    Now coil it around something like a pencil to the right length so that it will all fit into the reservoir.

    image

    If you have an LCR meter it can be tested before setting up the Arduino.  Here the capacitance is shown to be 61pF with the sensor out of the water.

    image

    Sticking the sensor into the water results in a measured capacitance of 123 pF.  Note that the end of the sensor needs to either be insulated or turned up so as to be kept dry as shown here.

    image

    Recall that in an RC Low Pass Filter the time constant is given by Tc = R x C.  Using that relationship and the ability of the Arduino to measure voltage and time a simple Capacitance Meter can be created as described here: https://www.arduino.cc/en/Tutorial/Foundations/CapacitanceMeter

    The Arduino code in the link above was modified by substituting micros() for millis() in the time measurement and the use of a 10M Ohm resistor since the DIY sensor has small capacitance and charges up fast.  The output to the serial monitor is shown below as the coil is inserted and removed from the water.

    image

    I didn't change the print statement so it says nanoFarads instead of picoFarads.  Note that it varies from 134 to 224 dry to wet which is more than what the LCR meter showed.  But it shows a clear and easily measured difference between dry and wet that could be calibrated.  Here it is plotted.

    image

    For those that require video, here you go:

    1321.IMG_7301.MOV

    This is the first thing that came to mind using the criteria that Andrew set out.  I've not tested repeatability or drift.  Another thing that might be done is just measure the temperature out as compared to the environment.  If it is cooler then presumably there is water evaporating and cooling the air if humidity is low enough. 

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to fmilburn

    Nice one Frank.  Even as I wrote my last post I started wondering if the water would make a useful dielectric and if so could we take a capacitance measurement.  Clever.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to Andrew J

    That is a nice succinct description of how it works 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to shabaz

    Also should mention (you probably already know, but to me it was non-intuitive initially) that you'll want to enable the humidity feature a bit intermittently once it starts getting hotter, to control it to a lower value (whereas originally I thought higher humidity as the temperature rises was better). Meaning, if you ordinarily like (say) 60% RH, then you might want it set to (say) 40% RH once the weather is hot, to keep the dew point value from going high, if we assume dew point to be a good indicator of personal comfort.

    I've never understood why typical home temperature/humidity sensors often don't display the dew point, whereas they have all the information to compute that. 

    The Mijia modules are pretty good (think I've mentioned them in the past), they use a nice Sensirion chip internally, and they are BLE-enabled, so a Pi etc can read off the temperature and humidity, compute the dew point and alert if it is out of the desired range.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to beacon_dave
    beacon_dave said:
    Some of the evaporative ones just blow air through a wicking filter or use ultrasonics or an impeller to create a mist that gets blown out by the fan.

    Yes I believe this is closer to how it works Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to beacon_dave

    Dang, no stock there. Must keep searching.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>