Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 414 subscribers
  • Views 5841 views
  • Users 0 members are here
  • help
  • prototyping
  • code
  • arduino
Related

Need help

masa98
masa98 over 4 years ago

hi

im working on a car seat controller and im using 2 arduino nano boards to controll the seat motors. but i ran into a problem with the code. i only get 1V from D2,D4,D5 if i use this code. but if i load another code the pins give 5V and my cirquit only draws 8.5 mA. can some body help.

 //B1-B6 Buttons 
 //D2-D7 output pins
 
int BI = 14;
int B2 = 15;
int B3 = 16;
int B4 = 17;
int B5 = 18;
int B6 = 19;

int D2 = 2;
int D3 = 3;
int D4 = 4;
int D5 = 5;
int D6 = 6;
int D7 = 7;

void setup() {
  
  pinMode(B1, INPUT);
  pinMode(B2, INPUT);
  pinMode(B3, INPUT);
  pinMode(B4, INPUT);
  pinMode(B5, INPUT);
  pinMode(B6, INPUT);

  pinMode(D2, OUTPUT);
  pinMode(D3, OUTPUT);
  pinMode(D4, OUTPUT);
  pinMode(D5, OUTPUT);
  pinMode(D6, OUTPUT);
  pinMode(D7, OUTPUT);
  
}

void loop() {
  
  if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) {
    
  digitalWrite(D2, HIGH);
  digitalWrite(D3, LOW);
}
  if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) {
    
  digitalWrite(D3, HIGH);
  digitalWrite(D2, LOW);
}
  else{
  digitalWrite(D2, LOW);
  digitalWrite(D3, LOW);
}

  if (digitalRead(B3) == HIGH && digitalRead(B4) == LOW) {
    
  digitalWrite(D4, HIGH);
  digitalWrite(D5, LOW);
}
  if (digitalRead(B4) == HIGH && digitalRead(B3) == LOW) {
    
  digitalWrite(D5, HIGH);
  digitalWrite(D4, LOW);
}
  else{
  digitalWrite(D4, LOW);
  digitalWrite(D5, LOW);
}

  
  if (digitalRead(B5) == HIGH && digitalRead(B6) == LOW) {
    
  digitalWrite(D6, HIGH);
  digitalWrite(D7, LOW);
}
  if (digitalRead(B6) == HIGH && digitalRead(B5) == LOW) {
    
  digitalWrite(D7, HIGH);
  digitalWrite(D6, LOW);
}
  else{
  digitalWrite(D6, LOW);
  digitalWrite(D7, LOW);
}
}

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 4 years ago +4
    It looks like the second 'if' should be an 'else if'. if else if else instead of if if else Otherwise the pin is being turned on by the first if and then immediately turned off by the else.
  • scottiebabe
    scottiebabe over 4 years ago +4
    'B1' versus 'BI' seems strange, not sure if it's related.
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps +4
    This is what happens: Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,D2: false ,D3: false , Condition: B1 : 0, B2 : 1 - D2: false ,D3: false ,D3: true ,D2: false , Condition: B1 : 1, B2 : 0 - D2:…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to masa98

    Did you change all occurrences of BI ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • masa98
    masa98 over 4 years ago in reply to Jan Cumps

    yes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to masa98

    This one

    int BI = 14;

    this one:

    if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) {

    and this:

    if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) {

    ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    ... and: are the buttons debounced?

    ... and what do you measure on D2 -> D4 if you all set them to HIGH, without doing any other logic?
    What are they connected too (schematic) ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • masa98
    masa98 over 4 years ago in reply to Jan Cumps

    the code looks like this and i still have the problem with D3 it gives only 2.9v when HIGH

     //B1-B6 Buttons 
     //D2-D7 output pins
     
    int Button1 = 14;
    int Button2 = 15;
    int Button3 = 16;
    int Button4 = 17;
    int Button5 = 18;
    int Button6 = 19;
    
    int D2 = 2;
    int D3 = 3;
    int D4 = 4;
    int D5 = 5;
    int D6 = 6;
    int D7 = 7;
    
    void setup() {
      
      pinMode(Button1, INPUT);
      pinMode(Button2, INPUT);
      pinMode(Button3, INPUT);
      pinMode(Button4, INPUT);
      pinMode(Button5, INPUT);
      pinMode(Button6, INPUT);
    
      pinMode(D2, OUTPUT);
      pinMode(D3, OUTPUT);
      pinMode(D4, OUTPUT);
      pinMode(D5, OUTPUT);
      pinMode(D6, OUTPUT);
      pinMode(D7, OUTPUT);
      
    }
    
    void loop() {
      
      if (digitalRead(Button1) == HIGH && digitalRead(Button2) == LOW) {
        
      digitalWrite(D2, HIGH);
      digitalWrite(D3, LOW);
    }
      else{
      digitalWrite(D2, LOW);
      digitalWrite(D3, LOW);
    
    
    if (digitalRead(Button2) == HIGH && digitalRead(Button1) == LOW) {
        
      digitalWrite(D3, HIGH);
      digitalWrite(D2, LOW);
    }
      else{
      digitalWrite(D2, LOW);
      digitalWrite(D3, LOW);
    }
    }
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    Here's the loop() with indentation.

    void loop() {
    
    	if (digitalRead(B1) == HIGH && digitalRead(B2) == LOW) {
    		digitalWrite(D2, HIGH);
    		digitalWrite(D3, LOW);
    	}
    	else {
    		digitalWrite(D2, LOW);
    		digitalWrite(D3, LOW);
    		
    		if (digitalRead(B2) == HIGH && digitalRead(B1) == LOW) {
    			digitalWrite(D3, HIGH);
    			digitalWrite(D2, LOW);
    		}
    		else {
    			digitalWrite(D2, LOW);
    			digitalWrite(D3, LOW);
    		}
    	}
    }

    I'll try and write a testbed, and see what happens in the four scenarios:

    B1 B2
    0 0
    0 1
    1 0
    1 1
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • masa98
    masa98 over 4 years ago in reply to Jan Cumps

    buttons get 5v from power source. they connect to A0 and A1 (with a pull-down resistor).

    i dont have anything connected to output at the moment. but if i set all outputs HIGH and delete all logic i get 5v from all outputs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    This is what happens:

    Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,D2: false ,D3: false ,
    Condition: B1 : 0, B2 : 1 - D2: false ,D3: false ,D3: true ,D2: false ,
    Condition: B1 : 1, B2 : 0 - D2: true ,D3: false ,
    Condition: B1 : 1, B2 : 1 - D2: false ,D3: false ,D2: false ,D3: false ,

    see how many times the same digitalWrite() is called, in  test 1, 2 and 4? 

    Test code. The testLoop() is the same logic as your loop():

    #include <iostream>
    #include <string>
    
    #define HIGH (true)
    #define LOW (false)
    #define D2 ("D2")
    #define D3 ("D3")
    
    bool digitalRead(bool value) {
    	return value;
    }
    
    void digitalWrite(std::string pin, bool value) {
    	std::cout << pin;
    	if (value) {
    		std::cout << ": true  ,";
    	} else {
    		std::cout << ": false ,";
    	}
    }
    
    void testLoop(bool B1, bool B2) {
    	std::cout << "Condition: B1 : ";
    	std::cout << B1;
    	std::cout << ", B2 : ";
    	std::cout << B2;
    	std::cout << " - ";
    
    
    	if (digitalRead(B1) == HIGH && digitalRead(B2) == LOW) {
    
    		digitalWrite(D2, HIGH);
    		digitalWrite(D3, LOW);
    	}
    	else{
    		digitalWrite(D2, LOW);
    		digitalWrite(D3, LOW);
    
    
    		if (digitalRead(B2) == HIGH && digitalRead(B1) == LOW) {
    
    			digitalWrite(D3, HIGH);
    			digitalWrite(D2, LOW);
    		}
    		else{
    			digitalWrite(D2, LOW);
    			digitalWrite(D3, LOW);
    		}
    	}
    	std::cout << std::endl;
    }
    
    int main() {
    	testLoop(false, false);
    	testLoop(false, true);
    	testLoop(true, false);
    	testLoop(true, true);
    	return 0;
    }
    

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to masa98

    OK, this isolates it to the code issue. See below:

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to beacon_dave

    void loop() 
    {
      if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) 
      {
        digitalWrite(D2, HIGH);
        digitalWrite(D3, LOW);
      }
      else if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) 
      {
        digitalWrite(D3, HIGH);
        digitalWrite(D2, LOW);
      }
      else
      {
        digitalWrite(D2, LOW);
        digitalWrite(D3, LOW); 
      }
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>