Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 414 subscribers
  • Views 5863 views
  • Users 0 members are here
  • help
  • prototyping
  • code
  • arduino
Related

Need help

masa98
masa98 over 4 years ago

hi

im working on a car seat controller and im using 2 arduino nano boards to controll the seat motors. but i ran into a problem with the code. i only get 1V from D2,D4,D5 if i use this code. but if i load another code the pins give 5V and my cirquit only draws 8.5 mA. can some body help.

 //B1-B6 Buttons 
 //D2-D7 output pins
 
int BI = 14;
int B2 = 15;
int B3 = 16;
int B4 = 17;
int B5 = 18;
int B6 = 19;

int D2 = 2;
int D3 = 3;
int D4 = 4;
int D5 = 5;
int D6 = 6;
int D7 = 7;

void setup() {
  
  pinMode(B1, INPUT);
  pinMode(B2, INPUT);
  pinMode(B3, INPUT);
  pinMode(B4, INPUT);
  pinMode(B5, INPUT);
  pinMode(B6, INPUT);

  pinMode(D2, OUTPUT);
  pinMode(D3, OUTPUT);
  pinMode(D4, OUTPUT);
  pinMode(D5, OUTPUT);
  pinMode(D6, OUTPUT);
  pinMode(D7, OUTPUT);
  
}

void loop() {
  
  if (digitalRead(BI) == HIGH && digitalRead(B2) == LOW) {
    
  digitalWrite(D2, HIGH);
  digitalWrite(D3, LOW);
}
  if (digitalRead(B2) == HIGH && digitalRead(BI) == LOW) {
    
  digitalWrite(D3, HIGH);
  digitalWrite(D2, LOW);
}
  else{
  digitalWrite(D2, LOW);
  digitalWrite(D3, LOW);
}

  if (digitalRead(B3) == HIGH && digitalRead(B4) == LOW) {
    
  digitalWrite(D4, HIGH);
  digitalWrite(D5, LOW);
}
  if (digitalRead(B4) == HIGH && digitalRead(B3) == LOW) {
    
  digitalWrite(D5, HIGH);
  digitalWrite(D4, LOW);
}
  else{
  digitalWrite(D4, LOW);
  digitalWrite(D5, LOW);
}

  
  if (digitalRead(B5) == HIGH && digitalRead(B6) == LOW) {
    
  digitalWrite(D6, HIGH);
  digitalWrite(D7, LOW);
}
  if (digitalRead(B6) == HIGH && digitalRead(B5) == LOW) {
    
  digitalWrite(D7, HIGH);
  digitalWrite(D6, LOW);
}
  else{
  digitalWrite(D6, LOW);
  digitalWrite(D7, LOW);
}
}

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 4 years ago +4
    It looks like the second 'if' should be an 'else if'. if else if else instead of if if else Otherwise the pin is being turned on by the first if and then immediately turned off by the else.
  • scottiebabe
    scottiebabe over 4 years ago +4
    'B1' versus 'BI' seems strange, not sure if it's related.
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps +4
    This is what happens: Condition: B1 : 0, B2 : 0 - D2: false ,D3: false ,D2: false ,D3: false , Condition: B1 : 0, B2 : 1 - D2: false ,D3: false ,D3: true ,D2: false , Condition: B1 : 1, B2 : 0 - D2:…
  • colporteur
    colporteur over 4 years ago in reply to shabaz

    I have used the approach you suggest in the past with great success.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<