Arduino Forum So why does the Arduino IDE connect to an Arduino using a different COM port each time a different one is plugged in, even tho each Arduino is plugged into the same USB connector to the PC ?
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
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 392 subscribers
  • Views 3249 views
  • Users 0 members are here
  • arduino ide
  • arduino
Related

So why does the Arduino IDE connect to an Arduino using a different COM port each time a different one is plugged in, even tho each Arduino is plugged into the same USB connector to the PC ?

robogary
robogary over 2 years ago

Curious minds want to know 

So why does the Arduino IDE connect to an Arduino using a different COM port each time a different one is plugged in, even tho each Arduino is plugged into the same USB connector to the PC ?

Is it related to he USB driver IC used on the Arduino board ? 

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 2 years ago +5 verified
    This is the case with most USB devices. The USB transceivers are coded with unique serial numbers, and because of that, the drivers caused them to be assigned a unique COM id. On my development system…
  • beacon_dave
    beacon_dave over 2 years ago in reply to colporteur +3
    If the device vendor ID, product ID and serial number match then it should in theory get the same virtual COM port assignment each time, assuming it isn't currently active. If you type: set devmgr_show_nonpresent_devices…
  • BigG
    BigG over 2 years ago +2
    Having switched over to Linux OS on my computer years ago, I no longer have to experience this Windows COM port comedy. On the Arduino side, there is a core header file "usbconfig.h" which contains the…