Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino As PC Fan Controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 418 subscribers
  • Views 4304 views
  • Users 0 members are here
Related

Arduino As PC Fan Controller

nicolaoscon96
nicolaoscon96 over 8 years ago

Hello there,

 

It's been a while to write here and I came back with a question. I want to build a fan controller for my desktop pc and I wanted to build it with an Arduino (Just add some modes like gaming for full speed, office use for lower rpm and less noise)>>Where I will be able to control by sending a  number for example 1 for gaming mode 2 for office<<. I found some online and they are really cheap but I wanted to experiment with that. So I wanted to ask is this possible? Can I control (4 fans) with an Arduino and get feedback from them about the RPM and the voltage if it possible(have it connected with USB on my computer and read the output in Arduino IDE)? The fans that am using are 3 pins (black-red-yellow).

 

Thanks

nicolaoscon96

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 8 years ago +7
    Hello, Honestly, the 8-bit microcontroller in Arduino won't have enough resources to do that. It only has 2 8-bit counters and one 16 bit counters. If you want to monitor 4 fans independently, you need…
  • shabaz
    shabaz over 8 years ago +6
    Hi Nicolas, If you want to do it accurately, as David says, you'll need different hardware. According to the link here: How PC Fans Work the three-wire fan uses it's third wire to provide speed feedback…
  • shabaz
    shabaz over 8 years ago in reply to gdstew +4
    Getting RPM feedback actually isn't the end goal. Why not sometimes actually try to understand the requirement, and form a more complete answer that helps the user? Just an opinion I've formed over the…
  • koudelad
    koudelad over 8 years ago in reply to mcb1

    Very good point, Mark.

     

    Of course, driving simultaneous 4 fans would expect to get 4 different temperature sensors and/or control inputs.

     

    Newer motherboards use 4-pin fans, at least for the CPU fan. And it is often a feature (and a must have for laptops) of the motherboard to not start itself, it there is no CPU fan present. So this could actually lead to either let the CPU fan to be driven by the motherboard, or somehow fake that there is an active fan. (Similar applies to a GPU fan.) All the chips (CPU, GPU, maybe southbridge) have integrated temperature sensors and there is not a better way to measure the temperature rise that directly from the inside of the silicon. All externally attached temperature sensors will perform worse - which could be crucial in these times of automatic short periods of rapid overclocking - probably CPU throttling.

     

    However, what could be easily achievable with Arduino is to do just a case ventilation, connect one or more fans is parallel and drive them as one channel at once.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 8 years ago in reply to shabaz

    "What's with the quote-marks around "opinion""

     

    It is an "opinion" that few in this discussion shared, at least about the topic under discussion and in other ones as well. Not surprised that you would

    "miss" that even after I explicitly pointed it out to you.

     

     

    "I didn't ask you for your formed opinion, nor to withhold it."

     

    I didn't ask for yours either and I don't see how it was helpful to anybody in this post, not sure why you do. As I already stated I don't really think my

    opinion of you is helpful here either.

     

     

    Speaking of issues:

     

    Why don't you stick to the topic at hand and actually answer the question about why you think an accurate description on the tach output of a fan

    and what was required to interface to it was not helpful to somebody who wanted to use it? As to integrating the tach output these are fairly short

    pulses spaced relatively far apart so it would take a while to settle to a fairly accurate reading and of course some method of calibrating the voltage

    to RPM conversion would also be required. David had already described the micocontroller hardware needed to use a pulse tach output (a 16 bit

    counter with capture) and that the Arduino did not have enough counters to do everything required in the original post. It requires no external

    circuitry other than a pull up resistor, is fairly easy to implement in software (I know, I've done it in 8051 assembly), and doesn't require calibration.

     

     

    P.S. Thanks for taking my responses completely out of context to the discussion that was ongoing at the time on that particular forum as I noted

    in one of those responses. There were more than one or two "crazies" on there at the time and I was not the only one to say so. I would also like

    to note that a few of those "crazies" managed to get themselves banned from this web site, and I didn't.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to gdstew

    It is clear how you felt about your peers at the time, and that's just one documented example.

    You might call them 'crazies', I'd say it says more about you that you're willing to write off people like that.

    Just an opinion (and not a particularly high one of you as a result).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to gdstew

    that a few of those "crazies" managed to get themselves banned from this web site, and I didn't.

    Actually there has only ever been one banning from element14 and it wasn't for that behaviour.

     

     

     

    All this petty arguing is not helping the OP.

     

    So can I suggest you start another discussion, where you can both discuss it.

     

     

    Thanks

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • tbitson
    tbitson over 8 years ago

    nicolaoscon96,

     

    Just a couple of minors notes about your comment:

     

    Most 2-wire fans these days are brushless DC. They stopped making fans with brushes years ago. Too expensive and noisy.

     

    About your arduino resource statement, I'm pretty sure an arduino can do a decent job. Since the temperature doesn't change very rapidly, you could set a counter to read one fans tach output, calc the desired PWM, set the corresponding pin's PWM, then move the counter the next fan. Using a round-robin approach like this, you could control as many fans as there are PWM pins (15 on a Mega). The processing needs are minuscule, and since the tach output is in the kHz region, counting pulses or measuring pulse width takes milliseconds.

     

    As as others have pointed out, the hardware interface is a bit more complex, but there's no reason an arduino couldn't handle the task.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • franzl123
    franzl123 over 6 years ago

    Here is exactly what you are looking for: https://nerd-corner.com/arduino-fan-controller/ It is a Arduino Fan Controller.

    I also made some updates and added a Bluetooth classic module. Then I programmed an android app and now I can control my fan via bluetooth: https://nerd-corner.com/android-bluetooth-classic-app-for-arduino-fan-control/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<