Arduino Forum Arduino gsm shield issue
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
  • Replies 7 replies
  • Subscribers 403 subscribers
  • Views 982 views
  • Users 0 members are here
  • gsmshield
  • uno
  • arduino
Related

Arduino gsm shield issue

tonderai
tonderai over 12 years ago

Hello

 

I recently bought the sim900 gsm module: http://www.ebay.co.uk/itm/GSM-GPRS-Shield-For-Arduino-/230911052682?pt=LH_DefaultDomain_0&hash=item35c35f0b8a

 

 

I have been working the https://code.google.com/p/gsm-shield-arduino/downloads/list using the arduino uno :https://www.dipmicro.com/store/BTE-RCB2011

 


I have configured every thing the right way and now trying the sms example. The serial
output says message sent but the message is not recieved by the phone. Hope you can help.

 

#include "SIM900.h"
#include <SoftwareSerial.h>
//If not used, is better to exclude the HTTP library,
//for RAM saving.
//If your sketch reboots itself proprably you have finished,
//your memory available.
//#include "inetGSM.h"

 

//If you want to use the Arduino functions to manage SMS, uncomment the lines below.
#include "sms.h"
SMSGSM sms;

 

//To change pins for Software Serial, use the two lines in GSM.cpp.

 

//GSM Shield for Arduino
//www.open-electronics.org
//this code is based on the example of Arduino Labs.

 

//Simple sketch to send and receive SMS.

 

int numdata;
boolean started=false;
char smsbuffer[160];
char n[20];

 

void setup()
{
  //Serial connection.
  Serial.begin(9600);
  Serial.println("GSM Shield testing.");
  //Start configuration of shield with baudrate.
  //For http uses is raccomanded to use 4800 or slower.
  if (gsm.begin(2400)){
    Serial.println("\nstatus=READY");
    started=true; 
  }
  else Serial.println("\nstatus=IDLE");
 
  if(started){
    //Enable this two lines if you want to send an SMS.
    if (sms.SendSMS("+444538590489", "Arduino SMS"))
      Serial.println("\nSMS sent OK");
  }

 

};

 

void loop()
{
  if(started){
    //Read if there are messages on SIM card and print them.
    if(gsm.readSMS(smsbuffer, 160, n, 20))
    {
      Serial.println(n);
      Serial.println(smsbuffer);
    }
    delay(1000);
  }
};

  • Sign in to reply
  • Cancel

Top Replies

  • theenggprojects
    theenggprojects over 10 years ago +1
    You should have a look at this link ..... http://www.theengineeringprojects.com/2015/02/receive-sms-commands-using-sim900-arduino.html .... It will give you the basic idea off how GSM works, it actually…
Parents
  • theenggprojects
    theenggprojects over 10 years ago

    You should have a look at this link ..... http://www.theengineeringprojects.com/2015/02/receive-sms-commands-using-sim900-arduino.html .... It will give you the basic idea off how GSM works, it actually works using AT commands sowhen you send the AT commands then it replies back so you should send the command then wait for the response, this link will help you as it has the code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • theenggprojects
    theenggprojects over 10 years ago

    You should have a look at this link ..... http://www.theengineeringprojects.com/2015/02/receive-sms-commands-using-sim900-arduino.html .... It will give you the basic idea off how GSM works, it actually works using AT commands sowhen you send the AT commands then it replies back so you should send the command then wait for the response, this link will help you as it has the code.