Arduino
  • Products
  • More
Arduino
Arduino Forum RGB LED night light
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 405 subscribers
  • Views 1136 views
  • Users 0 members are here
  • light
  • arduino_uno
  • night
  • leds
  • reg
Related

RGB LED night light

josh_j
josh_j over 12 years ago

Ok this is what I'm trying to do. I want to create a RGB LED night for my girlfriend using an Arduino and have the LEDs fade through different colors. I want to drive at least 6 LEDs. I've been talking to people on the Arduino Google+ group but this one guy gave me a schematic for my idea, but I'm really really new to all this. Is there a driver board for RGB LEDs that I can buy and use that and the Arduino to make this? I just want something that will do what I'm planning but is easy for newbies like myself. It would be cool too if the Arduino could detect the ambient light in the room and come on as needed. I would also buy a 9V wall adaper for so the Arduino could run off power from a outlit.

 

If someone on here is able to help me work through this project and give me ideas and easy ways of creating this for my GF that would be amazing!

 

P.S. I have a Arduino Uno

 

Thanks!

Josh

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to josh_j +1
    By chance did you look at the Adafruit tutorial.? I'm sure the fact you did the code (rather than have someone else supply) will impress you girlfriend. mark
  • ntewinkel
    ntewinkel over 12 years ago in reply to josh_j +1
    Cool project! You'd have to add the variable resistor to one of the analog inputs, and then use analogWrite to output to the LED. Oomlout has a basic example (See "Making it better, Control the Brightness…
Parents
  • billabott
    billabott over 12 years ago

    Step 1: Goto http://shieldlist.org/

     

    Step 2: Type in KeyWords for what you want.

     

    Step 3: Research and choose what it is you like.

     

    I would choose THIS or the current standard RGB LED Strip as seen on ebay, AdaFruit, and many others.

     

    2 hours later: Additionally, you may be looking for this one.

     

     

    - end of line -

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • josh_j
    josh_j over 12 years ago in reply to billabott

    This RGB LED Shield is exactly what I've been looking for! Now the next question I have is there scoure code to go with this? Also what can I do to defuse the lights so their a soft glow. Can I use a Cds cell so the Arduino Uno can sense ambient light?

     

    http://www.seeedstudio.com/depot/rgb-led-shield-v14-kit-p-430.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • josh_j
    josh_j over 12 years ago in reply to billabott

    This RGB LED Shield is exactly what I've been looking for! Now the next question I have is there scoure code to go with this? Also what can I do to defuse the lights so their a soft glow. Can I use a Cds cell so the Arduino Uno can sense ambient light?

     

    http://www.seeedstudio.com/depot/rgb-led-shield-v14-kit-p-430.html