Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino + two Bluetooth HC05
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 401 subscribers
  • Views 2523 views
  • Users 0 members are here
  • bluetooth
  • ld293
  • motors
  • hc05
  • dc
  • arduino
Related

Arduino + two Bluetooth HC05

Former Member
Former Member over 10 years ago

Hi everybody. (I am posting in the wrong place please move this topic where it should belong).

 

I am trying to control two DC motors remotely via bluetooth and I am facing a problem which is Arduino doesn't seems to be able to manage two SerialSoftware connexion at same time.

On my prototype breadboard the two motors and the two hc05 works fine as long as I only start one at time.

 

If the arduino cannot handle two serial connections I guess I have to use a 'middleware' component to mux/demux the serial data but I have no idea what component can do that. any idea how to achieve that ?

 

Attached the breadboard scheme I am using now and which is working fine (beside the fact that I can't rx/tx with two hc05

and the Arduino code I am using.

 

Thank you very much in advance for any little help on this.

Attachments:
image
Circuit24.ino.zip
  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    It would seem that two softwaresserial ports are available. Arduino - TwoPortReceive
  • neilk
    neilk over 10 years ago in reply to Former Member +1
    Hi bzhmaddog I was also going to ask why two Bluetooth modules, but gadget.iom beat me to it! I now understand your problem a little better now. gadget.iom has given you a link to two ports on Software…
  • Former Member
    Former Member over 10 years ago +1
    Thx for your answers all. I'll give a try to port1.listen/port2.listen tomorow (I am out of town till tomorow). I'll keep you up to date with a results
Parents
  • gadget.iom
    gadget.iom over 10 years ago

    Hi Cedric

     

    I'm curious as to why you are using two bluetooth modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 10 years ago

    Hi Cedric

     

    I'm curious as to why you are using two bluetooth modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 10 years ago in reply to gadget.iom

    Hi. The two motors are in fact two cars moving on two different tracks and therefore need to be controlled by two different smart phones.

    Since it is not possible to connect 2 devices to one hc-05 I have to use two separate modules.

     

    by cars moving on tracks I mean this kind of game > http://uncrate.com/p/2009/12/shelby-slot-car-track.jpg

     

    https://www.youtube.com/watch?v=9ZCZTW_K_zY

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to Former Member

    Ahh. That clarifies things slightly. image

    I was envisaging something like this:

    91050-Tamiya-Tracked-Vehicle-Chassis-Kit_Pic02.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to Former Member

    Hi bzhmaddog

     

    I was also going to ask why two Bluetooth modules, but gadget.iom beat me to it! I now understand your problem a little better now.  gadget.iom     has given you a link to two ports on Software.serial.

     

    I can assure you that you can also create 2 serial interfaces by using  pins 0 and 1 on the standard serial interface and a Software.Serial port.

     

    Incidentally, I noticed that in the code you supplied, 1 Software.serial port and its corresponding motor code was commented out. I assume you have demonstrated that the other half of your code also works?

     

    best wishes

     

    Neil
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.