Arduino Forum Arduino + two Bluetooth HC05
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
  • Replies 10 replies
  • Subscribers 401 subscribers
  • Views 2522 views
  • Users 0 members are here
  • bluetooth
  • ld293
  • motors
  • hc05
  • dc
  • arduino
Related

Arduino + two Bluetooth HC05

Former Member
Former Member over 10 years ago

Hi everybody. (I am posting in the wrong place please move this topic where it should belong).

 

I am trying to control two DC motors remotely via bluetooth and I am facing a problem which is Arduino doesn't seems to be able to manage two SerialSoftware connexion at same time.

On my prototype breadboard the two motors and the two hc05 works fine as long as I only start one at time.

 

If the arduino cannot handle two serial connections I guess I have to use a 'middleware' component to mux/demux the serial data but I have no idea what component can do that. any idea how to achieve that ?

 

Attached the breadboard scheme I am using now and which is working fine (beside the fact that I can't rx/tx with two hc05

and the Arduino code I am using.

 

Thank you very much in advance for any little help on this.

Attachments:
image
Circuit24.ino.zip
  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    It would seem that two softwaresserial ports are available. Arduino - TwoPortReceive
  • neilk
    neilk over 10 years ago in reply to Former Member +1
    Hi bzhmaddog I was also going to ask why two Bluetooth modules, but gadget.iom beat me to it! I now understand your problem a little better now. gadget.iom has given you a link to two ports on Software…
  • Former Member
    Former Member over 10 years ago +1
    Thx for your answers all. I'll give a try to port1.listen/port2.listen tomorow (I am out of town till tomorow). I'll keep you up to date with a results
Parents
  • dougw
    dougw over 10 years ago

    Another way to do this is to use an arduino Mega - it has 4 serial ports.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to dougw

    @Douglaswong > Arduino Mega would work. But considering the price of arduino Mega over Nano I would rather use two nano (since I don't care of the power consumption).

    I can get a nano for 14RMB (~2$) while a mega cost 58RMB (~9$)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to dougw

    @Douglaswong > Arduino Mega would work. But considering the price of arduino Mega over Nano I would rather use two nano (since I don't care of the power consumption).

    I can get a nano for 14RMB (~2$) while a mega cost 58RMB (~9$)