Arduino
  • Products
  • More
Arduino
Arduino Forum Push button to cycle through different modes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 413 subscribers
  • Views 1633 views
  • Users 0 members are here
  • mode_switch
  • button
  • arduino
  • shift_register
Related

Push button to cycle through different modes

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I am using the library from Elco Jacobs to control 8 RGB LEDs.

(ShiftPWM_Non_Blocking fromShiftPWM: the easiest software PWM library for Arduino | ElcoJacobs.com)

The sketch is awesome. It includ es 9 different modes for the LEDs and uses Serial.parseInt() to set the mode.

I built up the circuit on a perf board and want the whole system to be controlled by just 1 push button. I want the program to start when plugged in and stay in the first mode and switch to the second mode when the push button is pressed. Then, when pressed again, move to the 3rd mode then 4th ect.

I feel like this should be easy but I'm new to this stuff and I cannot find any help anywhere on this!

 

Thanks for any and all help.

 

 

/////This is the part of the sketch that selects the mode

 

void setup(){

  while(!Serial){

    delay(100);

  }

  Serial.begin(9600);

 

  // Sets the number of 8-bit registers that are used.

  ShiftPWM.SetAmountOfRegisters(numRegisters);

 

  // SetPinGrouping allows flexibility in LED setup.

  // If your LED's are connected like this: RRRRGGGGBBBBRRRRGGGGBBBB, use SetPinGrouping(4).

  ShiftPWM.SetPinGrouping(1); //This is the default, but I added here to demonstrate how to use the funtion

 

  ShiftPWM.Start(pwmFrequency,maxBrightness);

  printInstructions();

}

 

void loop()

{   

  if(Serial.available()){

    if(Serial.peek() == 'l'){

      // Print information about the interrupt frequency, duration and load on your program

      ShiftPWM.PrintInterruptLoad();

    }

    else if(Serial.peek() == 'm'){

      // Print instructions again

      printInstructions();

    }

    else{

      fadingMode = Serial.parseInt(); // read a number from the serial port to set the mode

      Serial.print("Mode set to ");

      Serial.print(fadingMode);

      Serial.print(": ");

      startTime = millis();

      switch(fadingMode){

      case 0:

        Serial.println("All LED's off");

        break;

      case 1:

        Serial.println("Fade in and out one by one");

        break;

      case 2:

        Serial.println("Fade in and out all LED's");

        break;

      case 3:

        Serial.println("Fade in and out 2 LED's in parallel");

        break;

      case 4:

        Serial.println("Alternating LED's in 6 different colors");

        break;

      case 5:

        Serial.println("Hue shift all LED's");

        break;

      case 6:

        Serial.println("Setting random LED's to random color");

        break;

      case 7:

        Serial.println("Fake a VU meter");

        break;

      case 8:

        Serial.println("Display a color shifting rainbow as wide as the LED's");

        break;        

      case 9:

        Serial.println("Display a color shifting rainbow wider than the LED's");

        break;    

      default:

        Serial.println("Unknown mode!");

        break;

      }

    }

    while (Serial.read() >= 0){

      ; // flush remaining characters

    }

  }

  switch(fadingMode){

  case 0:

    // Turn all LED's off.

    ShiftPWM.SetAll(0);

    break;

  case 1:

    oneByOne();

    break;

  case 2:

    inOutAll();

    break;

  case 3:

    inOutTwoLeds();

    break;

  case 4:

    alternatingColors();

    break;

  case 5:

    hueShiftAll();

    break;

  case 6:

    randomColors();

    break;

  case 7:

    fakeVuMeter();

    break;

  case 8:

    rgbLedRainbow(3000,numRGBLeds);

    break;

  case 9:

    rgbLedRainbow(10000,5*numRGBLeds);   

    break;  

  default:

    Serial.println("Unknown Mode!");

    delay(1000);

    break;

  }

}

  • Sign in to reply
  • Cancel
  • gadget.iom
    gadget.iom over 11 years ago

    Certainly should be possible.

     

    The following code sample should give you a good starting point. The number generated by this code can be used to represent a mode.

    Arduino - ButtonStateChange

    • Cancel
    • Vote Up 0 Vote Down