Arduino Forum Arduino as isp
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
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 2149 views
  • Users 0 members are here
  • isp
  • atmelstudio7
Related

Arduino as isp

strb
strb over 9 years ago

Hi, I have to use arduino uno as isp with atmel studio 7, I've upload on arduino the "arduinoasisp" sketch but i can't configure atmel studio to use it as the programmer, I've already found a couple of tutorial but it still doesn't work (probably I'm doing something wrong). Anyone can help me? Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 9 years ago +2 suggested
    gihu I have insert the attiny into arduino ide but but when I try to program it it doesn't work. However I have found another solution, it is a little more tricky but it works, it consist on macking the…
  • clem57
    clem57 over 9 years ago +1
    Sure. What steps did you take?
  • gihu
    gihu over 9 years ago in reply to strb +1
    Ciao Steffano, Have you checked this?: Arduino Playground - ArduinoOnOtherAtmelChips So, you can also try to use Arduino IDE if it is easier. Regards
Parents
  • clem57
    0 clem57 over 9 years ago

    Sure. What steps did you take?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    Sure. What steps did you take?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • strb
    0 strb over 9 years ago in reply to clem57

    On the menu tool> external tool I wrote the name in "title", the file path of "avrdude.exe" in "command" and I copied "-F -v -patmega328p -carduino -P.COM06 -b57600 -D -Uflash:w:"$(ProjectDir)Debug$(ItemFileName).hex":i -CD:/arduino-1.6.7/hardware/tools/avr/etc/avrdude.conf" in "arguents", then I tryed to flash a microcontroller with an example program but doesn't appear the external tool in the "device programming", i see only the simulator.

     

    The tutorial that I've found are these:

    https://asensar.com/blog/2013/how-to-integrate-avrdude-with-atmel-studio/

    Integrate ArduinoISP and Atmel Studio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to strb

    Before configuration, did you?

    Step 1: Download and Install Arduino IDE.

    If you don’t have it already you can download if from arduino.cc. I have installed Arduino IDE in D:/arduino-1.0.4

     

    Also use the Arduino IDE first as proof it is installed and functionally working.

     

    Clem