Arduino Forum HELP THIS BEGINNER PLZ
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
  • State Suggested Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 402 subscribers
  • Views 1534 views
  • Users 0 members are here
Related

HELP THIS BEGINNER PLZ

cannet
cannet over 6 years ago

Actually I'm new with Arduino so......

Can someone Help me with this program

I has seen error on line>>         Height=31-(ultrasonic.Ranging(CM));          <<

said that no has member named

 

#include <Ultrasonic.h>

#include <LiquidCrystal.h>

 

LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

Ultrasonic ultrasonic(A0,A1);

int Height;

 

void setup() {

    lcd.begin(16, 2);

     }

 

void loop()

{

  lcd.clear();

  lcd.print("Distance: ");

  lcd.print(ultrasonic.Ranging(CM));

  lcd.print("cm");

  lcd.setCursor(0, 1);

  lcd.print("Height: ");

  Height=31-(ultrasonic.Ranging(CM));

  lcd.print(Height);

  lcd.print("cm");

   

  delay(1000);

  }

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 6 years ago +3 suggested
    Do you also get the same error on the line “lcd.print(ultrasonic.Ranging(CM));” ? It could be that the Ultrasonic library that you are using does not have the Ranging function. I have seen at least two…
  • aswinvenu
    aswinvenu over 6 years ago in reply to aswinvenu +2 suggested
    Looks like the library that I have sent doesn't have the Ranging function. You can use this instead. https://www.itead.cc/blog/arduino-library-for-ultrasonic-ranging-module-hc-sr04 One possible reason…
Parents
  • aswinvenu
    0 aswinvenu over 6 years ago

    Hi Cannet,

     

    Looks like you didn't get the installation of the libraries right.

     

    Follow the below instructions:

     

    First you need to import the library so that the IDE recognizes it. The simplest way is importing through the IDE itself:
    - Click in ```Sketch > Include Library > Manage Libraries...```;
    - In the search field type: ```ultrasonic```;
    - In the list, look for ```Ultrasonic by Erick Simões```;
    - Click on ```Install```.

     

    You can also download the latest Ultrasonic library from the below link.

    https://www.arduinolibraries.info/libraries/ultrasonic

     

    Unzip it and read the README.txt.

     

    Before you write your own code, Please check the examples are running fine.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • aswinvenu
    0 aswinvenu over 6 years ago in reply to aswinvenu

    Looks like the library that I have sent doesn't have the Ranging function.

    You can use this instead.

    https://www.itead.cc/blog/arduino-library-for-ultrasonic-ranging-module-hc-sr04

     

    One possible reason for your error is you might have installed the wrong library (May be you installed the first library I sent and trying to call the Ranging funciton).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • aswinvenu
    0 aswinvenu over 6 years ago in reply to aswinvenu

    Looks like the library that I have sent doesn't have the Ranging function.

    You can use this instead.

    https://www.itead.cc/blog/arduino-library-for-ultrasonic-ranging-module-hc-sr04

     

    One possible reason for your error is you might have installed the wrong library (May be you installed the first library I sent and trying to call the Ranging funciton).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer