Arduino Forum Arduino soundpad suggestions for assignment
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
  • State Verified Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 401 subscribers
  • Views 1088 views
  • Users 0 members are here
Related

Arduino soundpad suggestions for assignment

fbirch
fbirch over 5 years ago

Hello everyone,

 

I'm hoping to use an arduino and some basic code in a group assignment and have zero experience with arduinos and very little coding knowledge.

 

I'd like to create an 8x8 grid of buttons that contain RGB lightning, and are attached to a speaker of some description to play a tone. The intention is to create a soundpad-esque (like a launchpad) tactile device that enables me to play a tone or series of tones when one of the buttons in the 8x8 grid are pressed. I'd also like to be able to have a colour displayed on the RGB lighting attached to the associated button.

 

I shall be using python to play a data value as a MIDI tone or series of tones, along with using a different data value to select a colour.

 

I am looking for hardware advice, as I have very little experience with Ardunio or circuitry in general. I will have access to a vast array of tools and five weeks to become competent enough to create such a project, along with a team of 5-8 people to assist. We are all in a similar boat with experience, however are eager to learn. I have already looked into multiple tutorials and other resources but it appears the options are near endless, so any assistance with recommendations or advice on this build specifically would be greatly appreciated.

 

Thank you for your time!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +5 suggested
    Hi Finn, This is quite general, I'm not sure what part you specifically need help with and I can't advise on your entire project. If you mean how to detect presses, then as you mention, buttons ( switches…
  • fmilburn
    fmilburn over 5 years ago +5 suggested
    Hi Finn, Expanding a bit on what Shabaz has outlined... Adafruit has a project which seems similar to what you have described: https://www.adafruit.com/product/1929 It is open source and there are links…
  • fmilburn
    fmilburn over 5 years ago in reply to fbirch +2 verified
    There is a fair amount of difference between Python and C / C++ as far as languages go, but Arduino is set up for beginners and isn't hard to learn. In my opinion C with some C++ is better suited to microcontrollers…
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    Hi Finn,

     

    Expanding a bit on what Shabaz has outlined...  Adafruit has a project which seems similar to what you have described: https://www.adafruit.com/product/1929


    It is open source and there are links to native format files for Eagle to create the hardware schematics and PCB. So you could recreate or modify it. Alternatively they sell the parts although they may not currently have all in stock. They supply code which uses Arduino which with a small amount of modification would work with any number of microcontrollers.

     

    I have played around with CircuitPython for making music and suggest using C / Arduino libraries instead. It may be possible to do it with CircuitPython but it does not implement interrupts and as Shabaz says there are less examples of use.



    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 5 years ago

    Hi Finn,

     

    Expanding a bit on what Shabaz has outlined...  Adafruit has a project which seems similar to what you have described: https://www.adafruit.com/product/1929


    It is open source and there are links to native format files for Eagle to create the hardware schematics and PCB. So you could recreate or modify it. Alternatively they sell the parts although they may not currently have all in stock. They supply code which uses Arduino which with a small amount of modification would work with any number of microcontrollers.

     

    I have played around with CircuitPython for making music and suggest using C / Arduino libraries instead. It may be possible to do it with CircuitPython but it does not implement interrupts and as Shabaz says there are less examples of use.



    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer