Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino based co2 dragster car timer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 417 subscribers
  • Views 1280 views
  • Users 0 members are here
  • start
  • timer
  • motion
  • stop
Related

Arduino based co2 dragster car timer

e14 Contributor
e14 Contributor over 13 years ago

My students are building a co2 dragster timer with an arduino and some hardware and lcd screen. Right now, we are using a laser pointer aimed at a photo resistor and when the beam is broken it starts the timer and same thing to stop the timer 50 feet away. The problem we experience is the reaction time of our system is two slow for the fast moving co2 cars. If we break the beam with our hand slowly it works fine but not quite good enough. The question is, what kind of sensor would be the best for sensing rapidly moving objects with a school budget in mind.

Tahnks

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago +1
    Carl I'd be trying an IR beam, and detector. They usually modulate the IR signal with 38Khz to avoid the ambient IR issues. Essentially you'd be looking for a constant 38Khz, so as soon as its gone its…
  • mcb1
    0 mcb1 over 13 years ago

    Carl

    I'd be trying an IR beam, and detector.

    They usually modulate the IR signal with 38Khz to avoid the ambient IR issues.

     

    Essentially you'd be looking for a constant 38Khz, so as soon as its gone its broken.

     

    You can place the sender and receiver in tubes, to cut done on the refection to improve accuracy.

     

    A quick check on Google gave 82,000 hits, but the first two are

    http://www.righto.com/2010/03/detecting-ir-beam-break-with-arduino-ir.html

     

    Terry King has a very good one with some easy to mount units.

    http://arduino-info.wikispaces.com/InfraredBeamPair

    http://yourduino.com/sunshop2/index.php?l=product_detail&p=86

     

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 13 years ago

    I think folks use infrared beam breaking for that kind of thing.

     

    Searching Google for "arduino infrared beam-break sensor" nets a fair number of examples.

     

    This seems to do what you need for just $16: http://yourduino.com/sunshop2/index.php?l=product_detail&p=86

     

    Otherwise maybe scavenging a set from an old garage door might work?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    use simple easily available IR modulator detector TSOP1738. This is universally used in most devices to receive IR codes from remotes.

     

    You can use and train your devices/car to read specific IR Codes to do control actions. Suggest you have a look at Ken Schrifft IR Library.

     

    Fairly easy to use the IR Library with TSOP1738 sensor

     

    Cheers

    sid

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    I think you've missed the point.

     

    They want to detect the car breaking a beam, and the LDR wasn't fast enough.

     

    Not sure how this fits that

    You can use and train your devices/car to read specific IR Codes to do control actions. Suggest you have a look at Ken Schrifft IR Library.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    hi marks,

     

    surely missed the point, it is object detection (IR Beam) with LDR....

     

    maybe a photo diode/photo transistor replacement would be an alternative..

     

    cheers

    sid