Arduino Forum DSM2 transmitter attached to Arduino via RS-232
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
  • State Not Answered
  • Replies 15 replies
  • Subscribers 404 subscribers
  • Views 1844 views
  • Users 0 members are here
Related

DSM2 transmitter attached to Arduino via RS-232

roineust
roineust over 12 years ago

Hello!

 

I would like to connect an Arduino Uno via RS-232,  with this transmitter:


http://www.micronradiocontrol.co.uk/docs/dt/dt-tx1-k1-1.pdf


And to have as servo controller, on the receiving side, this receiver:


http://www.hobbyking.com/hobbyking/store/__28554__OrangeRx_R615_Spektrum_JR_DSM2_Compatible_6Ch_2_4Ghz_Receiver.html

 


Can anyone instruct me with such a project?


Thanks a lot!

Roi Neustadt.


  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 12 years ago

    This is a big challenge.  Please review the MAX232 IC data sheet and see if you can manage it.

    Do a search using Google and YouTube for MAX232 and Arduino.  I think you may find what you need.

     

    Happy Trails.

     

    Ha.  The OP caught me shooting from the hip and missing the target completely.  Good call, OP.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • roineust
    0 roineust over 12 years ago in reply to billabott

    Hey Bill!

     

    I want my computer to connect to the Arduino via a USB cable, only for the sake of uploading the code and the Tx1-K1 DSM2 transmitter to connect to the Arduino, using the Arduino  TX and PWM pins using the RS232 protocol.

     

    I think there is no need in this project to connect the Arduino directly to the computer using the RS232 protocol or RS232 hardware.

     

    Have i misunderstood anything?

     

    Thanks a lot,

    Roi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 12 years ago in reply to roineust

    Let's see there are two distict features that make up RS-232 specification.  One is the well known 8-N-1 at a given baud rate which is 115200 according to the data sheet pdf you provided the link to.  And then there is the electrical signal level for which binary 0 is -8 V and binary 1 is +8 V.

     

    Your TX does not seem to work with true RS-232 signals.  Having located and read a document from the OEM's website, I have come to the conclusion that you REALLY need to read it too.  Especially, Section 4 which shows how to feed pin 7 (or 8).  http://www.deltang.co.uk/tx1-112.htm  This MAY NOT be the correct document for your TX.  If that is the case then please do tell me which is the right one.  Pay attention to the power supply requirements and there will be no tears because the TX got tore up.  Since the Uno is 5 V on a high (binary 1) you REALLY must understand and follow what the OEM shows about the interface between the Uno's output pin and pin 7 (or 8) of the TX.  Again, I point you to Section 4.

     

    I don't know but the answer you are looking for may be how to create and send the PPM signals into pin 7 (or 8) of the TX.  For that, I refer you to the Arduino Forum.  http://forum.arduino.cc/index.php?PHPSESSID=g7vue61elc4pk3312kt7uvrtl6&topic=146982.0  ,  http://forum.arduino.cc/index.php?PHPSESSID=g7vue61elc4pk3312kt7uvrtl6&topic=146982.0 and other discussions posted there that may be easily be found by inputting "ppm tx rc" into the search box on the Arduino Forum's pages.  Where you might learn that PPM is only between the TX and RX.  Ha, gotcha!

     

    Does your difficulty lie with creating, maintaining, and TXing a required 16 byte array?

    Byte 1 Checksum (sum of bytes 2-16 cast to 1 byte)

    Byte 2 Not used (can be any value)

    Bytes 3-16 2 bytes per channel with following structure 0b000 CCC PPPPPPPPPP    for a total of 16 bits which is 2 bytes

    - 000 = not used (normally zeros)

    - CCC = channel number (0b000=Thr, 0b001=Ail, 0b010=Ele, 0b011=Rud, 0b100=Gear, 0b101=Aux1, 0b110=Aux2)

    - PPPPPPPPPP = 0b0000000000 <= 10bit channel position <=0b1111111111

     

     

    Happy Trails

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 12 years ago in reply to billabott

    billabott wrote: And then there is the electrical signal level for which binary 0 is -8 V and binary 1 is +8 V.

     

    The actual RS232 specification for logic levels is binary 0 is minimum of -3V (maximum is -15V) and binary 1 is minimum of +3V (maximum is +15V).

    Many RS232 recievers will accept  0 V as a binary 0 although this is clearly out of spec.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 12 years ago in reply to billabott

    billabott wrote: And then there is the electrical signal level for which binary 0 is -8 V and binary 1 is +8 V.

     

    The actual RS232 specification for logic levels is binary 0 is minimum of -3V (maximum is -15V) and binary 1 is minimum of +3V (maximum is +15V).

    Many RS232 recievers will accept  0 V as a binary 0 although this is clearly out of spec.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billabott
    0 billabott over 12 years ago in reply to gdstew

    Thanks, Gary.  I was just quoting something (dated) I read the other day.  Wikipedia is my friend, too.