Arduino Forum serial monitor locks after exceeding threshold
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
  • State Verified Answer
  • Replies 18 replies
  • Answers 3 answers
  • Subscribers 403 subscribers
  • Views 1104 views
  • Users 0 members are here
Related

serial monitor locks after exceeding threshold

Former Member
Former Member over 12 years ago

My pro mini is writing values from a photocell to the serial monitor, reading correctly until exceeding the threshold, then stops and will not restart, even when the cell is returned to darkness. Assuming this is a software error. Would appreciate advise. Thanks.

 

#include <Stepper.h>

 

 

#define STEPS1 200

#define STOP 0

 

 

int rightSwitchPin =7;

int leftSwitchPin =8;

int sonarPin = A0;

int sonarValue = 0;

 

 

Stepper stepper1(STEPS1, 3,5,4,6);//bipolar

 

 

void setup()

{

  stepper1.setSpeed(30);

  Serial.begin(9600);

 

}

void loop()

{

  sonarValue = analogRead (sonarPin);

// Serial.println (sonarValue);

  delay(500);

 

 

  if (sonarValue >900)

  {

    Serial.println (sonarValue);

    while (digitalRead(rightSwitchPin) == LOW) //keep going until limit switch reached

    {

      stepper1.step(-1);  //move right

    }

    while (digitalRead(leftSwitchPin) == LOW) //keep going until limit switch reached

    {

      stepper1.step(1);  //move left

     

    }

  }

  else

  {

    stepper1.step (STOP);

  }

}

 


  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to Former Member +2
    Keith As Nico says ... Not sure where your sketch is, but you read the sonarValue at the start of the loop, then don't read it again until you hit the limit switch. The serial.println(sonarvalue) will…
  • billabott
    billabott over 12 years ago +1
    Have you tried changing the while statements to if statements?
  • Former Member
    Former Member over 12 years ago in reply to ntewinkel +1
    Thank you. After adding a println in each while statement, the sketch works fine. Had some help here. Keith
Parents
  • billabott
    0 billabott over 12 years ago

    Saying the LDR is wired with a pull down resistor does not give me the level of detail I expected.  Where is A0 and +5 V connected, eh?

     

     

    Back in the old days before integrated ADC the LDR would be used in this fashion.  http://www.rentron.com/micro-bot/images/CDS_Circuit.gif

     

    The discussion about that style of implementation is found here: http://www.rentron.com/micro-bot/cds.htm .

     

    Happy Trails

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • billabott
    0 billabott over 12 years ago

    Saying the LDR is wired with a pull down resistor does not give me the level of detail I expected.  Where is A0 and +5 V connected, eh?

     

     

    Back in the old days before integrated ADC the LDR would be used in this fashion.  http://www.rentron.com/micro-bot/images/CDS_Circuit.gif

     

    The discussion about that style of implementation is found here: http://www.rentron.com/micro-bot/cds.htm .

     

    Happy Trails

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer