Project stairs:
Stairs from underneath.
~Specs:
I have purchased nothing yet.
Item starter list:
Raspberry Pi
Ardunio (max) (I would like 12 "keys" or active stairs min)
sensors - tbd
The sensing is going to be the hard part (I think):
FSR: I started looking into force sensing resisters to be put under the laminate flooring but from googling and reading I'm uncertain that would work well.
PIR motion sensors issues/questions:
From looking on youtube most of the PIR sensors either have 2 short a sensing range or too large a range. 10cm to 15cm would probably be idea.
The "reset" time on PIR's factory preset?
If someone tried to key a stair twice quickly it would probably not activate for 2+ seconds?
IRDS: Thoughts on using IR distance sensor instead of PIR?
IR has the right range settings from 4 inches (10 cm) to 80cm.
IR Beam: Beam sensor would be too difficult to install due to the physical requirements of access to both sides of the stairs.
I'm assuming that I can get the sensed activation from the Ardunio to the rPI to play a note or tone?
Would this setup be able to trigger multiple notes at once? Lets say 4 feet(2 people) playing.
Thoughts on if this project is worthwhile?